Massimo,
Are you asking about the ADS8678 ADC? I'm not to familiar with this device. If you need some guidance working with it, post back to the forum with a new thread and another apps engineer will pick it up.
Joseph Wu
Hi,
Just noticed a section on the board that says the following:
Installed Device:
ADS8688
ADS8678
ADS8668
ADS8688A
ADS8698
There is a red mark next to ADS8698 while only white ones next to the others so I assume it is ADS8698?
All the best,
Davi…
Hi Dale,
thank you for the driver. Now I have a new problem (see screenshot) .
Here is the content of the file:
[ADS8664EVM] ID = "ADS8664 EVM" Resolution = "12" No.of Channels = "4" [ADS8668EVM] ID = "ADS8668 EVM"…
Part Number: ADS8674 Other Parts Discussed in Thread: ADS8678 Hey guys,
I am working with the ADS8678 EVM and appear to be having some issues with the communication. I have the board configured with default jumper settings and the GUI recognizes that…
Part Number: ADS8688EVM-PDK Other Parts Discussed in Thread: ADS8688A , ADS8664 , ADS8668 , ADS8674 , ADS8678 , ADS8684 , ADS8688 I am trying to install the software from the micro SD card, but, Windows sees the card as not formatted, so, I can not load the…
Hello user4076865,
Firstly, the amplifier U4 on your board was bypassed and you did not use the front-end amplifier because the default jumper on J8 is short between pin 2 and 3 also J25 is open which means the signal is not connected to the amplifier…
Part Number: ADS8674 Other Parts Discussed in Thread: ADS8678 Hello E2E,
I Looking for EVM of ADS8674, I could not find it. Is it possible to evaluate ADS8674 on the ADS8678 EVM by implementing ADS8674? Is GUI saported for ADS8674? Regards, ACGUY
Part Number: ADS8674 Other Parts Discussed in Thread: ADS8678 The SPI signals for an ADS8674/ADS8678 device are connected to GPIO lines on a processor and controlled through software to implement the SPI protocol for the device. After power on, the first…
Hi Tom
ADS8678 can support 0 to 10V input range. For unipolar applications ADS8678 input can be configured from 0V to 2.5 x VREF, 0V to 1.25 x VREF, 0V to 0.625 x VREF,0V to 0.3125 x VREF. ADS8678 has 4.096V internal reference.
ADS8678 EVM GUI allows you to…
Other Parts Discussed in Thread: ADS9110 , ADS8678 , THS4551 , THS4521 We are only able to record a peak measurement of 65,300 ADC (~2.245 V) with the ADS9110EMV development unit.
We have verified that our detector is putting out voltages, depending on our…