Part Number: ADS8681EVM-PDK Other Parts Discussed in Thread: ADS8681 Dear Support,
I am writing to seek assistance regarding the evaluation board ADS8681. While conducting tests with the SPI command, I observed an issue related to the board's functionality…
Part Number: ADS8681 Other Parts Discussed in Thread: ADS9226 Hi team,
If I have a differential output signal (voltage sensing from the AMC33x), and since this device has a single-ended input, how can I make use of the full dynamic range instead of only…
Part Number: ADS8681 Hello -
Looking for advice on how to connect the GND pad of the WQFN package - I have separated power rails and GNDs connected through a single jumper, effectively splitting the GND connections into an Analog and Digital GND. Which…
Part Number: ADS8681 Other Parts Discussed in Thread: DRV5056 , Hi,
I am looking to use DRV5056 chip at 5V and taking its output to ADC to SPI chip.
Q1: Can i drive ADC to SPI - AVDD at 5V and DVDD at 3V?
Q2: Will there be any constraints?
Q3: Is this typical…
Part Number: ADS8681 Hello.
I want to receive the output of ADS8681 in 1 MHz cycles
I am inquiring about the SPI configuration for the maximum output of ADS8681( 1 MHz ).
In the datasheet, maximum SPI clock is 66.67MHz(about 15ns).
Using the maximum clock…
Part Number: ADS8681 Hi Experts,
Good day. Hoping for your guidance to help me understand the input voltage range/operation of the ADC device ADS8681.
How is it possible that this able to measure bipolar voltage (i.e.+/-10V) input signal where in fact…
Part Number: ADS8681 Hello Team,
I'm posting this on behalf of my customer.
ADS8681 configured work with bipolar voltage, range +/-0.625*Vref. All configuration registers are programmed accordingly. It converts DC very well. However, I missed something…
Part Number: ADS8681 I'm trying to simulate a circuit that is connected to above mentioned ADC in Keysight ADS. since I cannot leave the circuit unconnected, I connected a 1MOhm resistor shunt to the ground to represent the ADC's input. please let me…