Part Number: ADS8688AT When ADS8688AT is unpowered (AVDD=DVDD=0V, and hence Vref_internal=0V), will the IC be damaged if the AUX_IN sees non-zero voltage? If not, what is the max input current rating on AUX_IN to have no damage to the IC?
Thank you in…
Part Number: ADS8688AT Other Parts Discussed in Thread: ADS8688 , Hi,
I have a couple questions regarding ADS8688 AUX_IN input voltage range.
(1) When using Vref_internal, can I assume that Vref_internal would be 0V when AVDD < 4.75V?
(2) Now say…
Part Number: ADS8688AT Hi Team,
I would like to confirm if part ADS8688AT is a cold parable. Can the IC handle inputs (AIN, AUX_IN, SPI, etc) without either or both AVDD and DVDD?
Thanks in advance.
Regards,
Marvin
Part Number: ADS8688AT
Dear team,
Our team is using ADS8688ATDBT in our designs, and we have some questions about the Idvdd_dyn parameter in the datasheet .
Datasheet is stating Idvdd_dyn=0.5mA when output is 0000h. Is this "dynamic" or "static" current…
Part Number: ADS8688AT Hello Everyone,
I am using ADS8688ATDBT in my design for converting Analog DC Voltage to Digital values. In the datasheet I found that the internal reference voltage for ADC IC is 4.096V.
In my design Input DC voltage is ranges from…
Part Number: ADS8688AT Other Parts Discussed in Thread: ADS8688 Hi experts!
My customer has the following question about the ADS8688AT:
We’ve been interested in using AD8688 for some low frequency signal processing. But, we’d like to do some differencing…
Part Number: ADS8688AT Other Parts Discussed in Thread: ADS8688 Hello team,
I need IBIS Model for the Part no. - ADS8688AT. Please Provide me with the same ASAP.
Thank you
Santhosh Kumar S
Part Number: ADS8688EVM-PDK Other Parts Discussed in Thread: ADS8688AT We recently received an evaluation board kit for ADS8688AT and after installing software that goes with it, I am not able to pass the "Connecting Hardware".
I can see the…
Hi Gerald,
ADS8688AT was just an example of a bipolar ADC.
If you want to sample a bipolar input signal using an F2837x device, you'll need to use some signal conditioning circuits to add an offset (and potentially scaling) before sampling it with the…