Part Number: ADS8689 Tool/software: Hello,
I am currently working on a project using a PIC16F15356 microcontroller and the ADS8689 ADC to read 8-channel 4–20 mA current signals through a MUX, and send the data to a PC via Modbus.
The communication…
Part Number: ADS8689 Other Parts Discussed in Thread: MUX36S08 , Tool/software: Hello, I am currently a student studying PIC microcontrollers.
I'm working on a project and having difficulties with the SPI communication part, so I’m writing to kindly…
Part Number: ADS8689 Tool/software: Hello,
We are redesigning an existing design using ADS8689 retaining the existing module specifications.
Following are the specification and Implementation details.
Input signal range: 1 to 5V, 0 to 5V, 0 to…
Part Number: ADS8689
Dear Technical Support Team,
Q1.
Could you tell me the maximum Io values for the “SDO pin” and “GPO pin.”?
Since the datasheet only listed the conditions mentioned below.
I could not find any information in the datasheet…
Part Number: ADS8689 Other Parts Discussed in Thread: ADS8681WEVM-PDK
Dear Technical Support Team,
I have questions about ADS8689.
Q1
In sections 6.5 through 6.10, the specifications are listed under the condition that DVDD = 3.3 V. If the conditions…
Part Number: ADS8689 In a new analog input board we use ADS8689IPW A/D converter.
During debugging we noticed a strange behaviour of converted values: (only) at certain levels of input voltage the converted points have an everage value (the expected…
Part Number: ADS8689 Hi everyone,
Refering to: www.ti.com/.../sbaa551.pdf
I'm designing an analog input module following this document, in my implementation I only need the single ended solution, can I just bypass the amplifier connecting directly…
Part Number: ADS8689 Tool/software: Dear , Data converters Support team. According to the datasheet, the Absolute Maximum Ratings of the ADS8689 are +7V for both AVDD and DVDD. The Recommended Operating Conditions for DVDD are up to AVDD.
Are there…
Part Number: ADS8689 Tool/software: While used in any range its not reading -ve voltages above -4V even in +/-12V range, right now I'm using +/-6.144 range positive range is fine but in negative range it's not reading above -4V i have 4 IC's but in every…
Part Number: ADS8689 Other Parts Discussed in Thread: OPA320 , ADS8509 Tool/software: Hi,
I have a ADC design, based on the ADS8689IPW to measure a +/-800Vdc voltage connected to a 200:1 voltage divider. (We need to measure negative voltages to detect…