Part Number: TMS320F28379D Other Parts Discussed in Thread: ADS8694 , C2000WARE Dear people,
please, it would be great if somebody could give me advise on this:
I am trying to communicate with a ADS8694 4 channels 18bit ADC via Spi, controlled by a TMS320F28379D…
Part Number: ADS8694 Other Parts Discussed in Thread: INA240 , OPA320 , ADS8914B , THS4551 Hi,
We are working on a MPPT Buck converter with a high accuracy required (1%) on global system.
So we are looking for a solution in order to reach an accuracy of…
Part Number: ADS8694 Hello, i have a question about the internal reference...
I guess its build from AVDD, which is 5V normally. How is the ref related to the stability of AVDD?
AVDD is generated with a transfomer and i have some noises on 5V supply. …
Part Number: ADS8694 Hi all, I have some question about the alarm feature of ADS8694. In the datasheet 8.3.11, the alarm signal will be triggered when an alarm condition is encountered for a particular channel. But the resolution of the ADC is 18 bit…
Other Parts Discussed in Thread: ADS8688 , ADS8664 , ADS8674 , ADS8684 , ADS8684A , ADS8694 , ADS8668 , ADS8678 , ADS8688A , ADS8698 Hi ti
Could you help to provide some ADC chipset with linux driver(better to have linux source code)? CPU is am571x。
spec
14bit…
Hi user6494725,
110ksps data rate is critical for Delta-Sigma ADCs including ADS1263. If your voltage inputs are single-end signals(I believe so). ADS8484A (16-bit) or ADS8694 (18-bit) will be a simple and precision solution which can meet all your requirements…
Other Parts Discussed in Thread: TIDA-01333 , TIDA-00764 , TIDA-00170 , ADS8688A , TIDA-010008 , ADS8694 , ADS8684 , ADS8688 , ADS125H02 , MUX36D04 , MUX509 , UCC12040 , SN6505B , UCC12050 Hi
We are designing Analog input module for following requirements.
Universal…
Part Number: ADS8698 Other Parts Discussed in Thread: ADS8694 , My ADS8694 is not responding on SPI, similiar to this question:
The platform is Raspberry PI 4, and on this platform, the SPI writes are per byte, and the clock stretches in between the bytes…
Hello Alexandre,
The AIN_xGND pin is limited to below range, you can not do this, otherwise, the ADC may be damaged because the signal to AIN_xGND has violated the Absolute Maximum input range. ADS8694 can be used to meet your requirement which is pin…