Part Number: ADS8698 The ADS8698 is already used for a new design in a high voltage power supply unit and works very well. But there is one feature of this ADC i missunterstood and therefor one important feature of our PSU will not work - the software…
Part Number: ADS8698 Hello? I am a Ph.D. student in electrical engineering. I am currently trying to change the input voltage range using ADS8698. Below is the link to the data sheet for the part I'm using. The figure below is the FSM illustration shown…
Part Number: ADS8698 I am using ADS8698 ADC in the range of 0-5 V. At one of its input the voltage given is +5V however it is making the digital data for 2.5V.
What may be the reason?
Part Number: ADS8698 I am using ADS8698 ADC using SPI and working correctly at ambient temperature. But when I operate at 71'c, the device reads approximately double range constant output even the input is varied. Please help to solve this issue. It's…
Part Number: ADS8698EVM-PDK i test a ads8698 evm gui and the program is stuck in program reset. the message says "Device is in Reset state. Uninstall Jumper J3". even if i open the jumper j3. i think it is problem of my ads board.
is it problem…
Part Number: ADS8698 Other Parts Discussed in Thread: ADS8588S My customer is asking the following question:
Figure 27 of the ADS8698 shows the error vs. source resistance. How far past 20 kohms can this graph be extrapolated linearly?
Can you comment…
Part Number: ADS8698 Hello,
looking at the ADS8698 datasheet, I can see on page 3 & 4 that REFSEL is located on pin 4 and DAISY is pin 3.
On the other hand, on the layout example (figure 112, page 68) I see that REFSEL is pin 3 and DAISY is pin 4…