Part Number: ADS8861 Other Parts Discussed in Thread: ADS8881 Hello, Our customer has two questions about ADS8861/81. 1. Is there any way to reset internal clock count of SCLK? I mean that is it possible to use ADS8881 as 16bit ADC?
2. Could you tell me input…
Part Number: ADS8861 Hello,
I have two question for ADS8861.
1. Does ADS8861 have S/H capacitance reset function that discharges the capacitance before starting next sampling?
2. I think usually a certain level of previous sampled voltage remains in S…
Part Number: ADS8861 The input range is -Vref ---+Vref , If could i set the the Vref is 0V-5V / then input is,0V--+5V ? If set Vref is -5V---+5V, the input range is -5V---+5V?
what is the Analog input impedance of ADS8861?
Hello,
This software is not supported in windows 10. It seems like the main issue is due to driver signing. Some have had luck in the following threads:
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/594593/ads8861…
Part Number: ADS8861 Other Parts Discussed in Thread: ADS8881EVMV2-PDK Hi,
I am currently trying to use the ADS8861EVM for a project but the ADC pro driver software is unavailable. Is there a way to have access to the this driver so I can evaluate using…
Part Number: ADS8861 Hi E2E,
Good day.
In implementing the daisy-chain mode with a busy indicator for ADS8861, here are some questions:
1. Referring to the interface timing diagram in figure 63, when to interrupt on the falling edge?
2. How does the digital…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS8861 , , ADS8363 , ADS8556 , ADS8910B Hi team,
My customer Qunling is working on a project. In this project, they get four signal need to be sampled, one high speed signal, grid current、voltage、one…
Part Number: ADS8860 Other Parts Discussed in Thread: REF6250 , LM4120 , REF6050 , ADS8861 , OPA376 , THS4551 , LM7705 , OPA320 Hi,
I wonder if anyone can help me. I am using the ADS8860 ADC and some of the boards I have had manufacturered are exhibiting a minimum…
Part Number: ADS8860 Other Parts Discussed in Thread: ADS8861 Hi team,
We can saw that our ADS8860 is for single-ended input.
But the pin have AINN & AINP, is that means this device can also use for differential input?
Which one do we recommend?
…
Part Number: ADS8861 Other Parts Discussed in Thread: TIPD115 Tool/software: Code Composer Studio Hello,
I'm working with ADS8861 on a project to acquire analog variables. As a test, I am converting a 50 Hz signal with a sampling frequency of 5 kHz…