Other Parts Discussed in Thread: ADS8864 , ADS7042 Hi,
I am working on a design with and ADS8864. The analog section has some signal condition with a couple of amplifiers and a voltage reference with no shutdown pins. The problem is, I need to shut down…
Other Parts Discussed in Thread: ADS8864 , ADS8685 Hi team,
Customer is looking for SAR ADC. The requirements are below.
Single End input, 0~5V input range, VDD=5V, single ch, 400~500kSPS, 16bit.
Customer prefers ADC integrating OAPMP like ADS8685 because…
Part Number: ADS8664 Other Parts Discussed in Thread: ADS8864 , Hi experts,
My customer was evaluating ADS8664 and found ADS8864 is easy to reset 。 could you please check their design and help to comment how to improve this ?
thanks.
Part Number: ADS8339 Other Parts Discussed in Thread: REF5045 , THS4281 , , REF3240 , OPA140 , ADS8864 , REF6045 , OPA350 Hi Team,
1. In the ADS8339 EVM, REF5045 is buffered by THS4281 then sent to the REF pin of ADS8339. I'm also aware that our REF6xxx family…
Hello Y.Ottey,
You do not need to use daisy-chain mode to get simultaneous sampling. You can connect the CONVST of 53 devices together (the host MCU Output pin must drive this load) and all 53 devices will then simultaneously sample their respective inputs…
Hi Ken,
ADS8515 does not fit your new requirement, it has a internal 4.096V voltage reference with a very narrow range(4.076V to 4.116V). Also, the external reference voltage range is from 3.9V to 4.2V(4.096V typ is expected as well).
There are two solutions…
hi Vahid,
I just got back from my long absence...
I talked with the BU folks and actually you may want to consider the ADS8864 (instead of ADS8865).
The ADS8864 supports single-ended input and you don't need to use a single-ended to differential circuit…
Hello Shinichi,
I will need to investigate to see if we can get some exact numbers, but maybe this will help.
1. DCLOCK can be as low as 24kHz, so the delay between CS going low and the first clock rising edge in this case is ~1/Fs, or 41.5uS. The datasheet…
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8864 We want to use A 16-bit ADC,now we are evaluating ADS8866, I want to ensure that After the first byte sample is completed, can I restart the AD transform before the second byte sample ?
Takumi-san,
I don't see too many options for an LTC2312-14 replacement. However, I did see some that might be made to work.
The TLC3541, the ADS8319, and the ADS8864 all are similar parts. However these would also need an external reference. Most…