Part Number: ADS8866 Other Parts Discussed in Thread: RCV420 Tool/software: Hi folks!!
I have 3 questions regarding this AD converter:
1) In the spec it says that the mininum clock frequency is 16MHz. Is it possible to use Raspberry Pi 4 to conect it…
Part Number: ADS8866 Tool/software: Now, I am getting conversion results from an ADS8866 in 3-Wire nCS Mode under microcontroller control.
(SPI_COMM_MODE1 = CPOL=0, CPLA=1)
The gain error in the conversion results is 7%, which seems to be much larger…
Part Number: ADS8866
Hi team,
My customer considering using AVDD=DVDD=+3.3V±5% and VREF=5V±5% in customer application. However, there is a discrepancy in the datasheet between NOM=+5V at 7.3 and MAX=+5V at 7.5, and My customer unsure whether…
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8689 Hello team,
I have a question about ADS8866. Could you please help me with the answer?
Currently, there are customers who want to use products with Ads8866 at high temperatures. The operating…
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8320 Hello I want to know about ADS8866 specification.
The ADS8866 datasheet lists only operating ambient temperature (free-air temperatrue (Ta))
I want to know the Junction Temperature (Tj) and…
Part Number: ADS8866 Hi Team,
I have two questions about ADS8866. Could you help me with the answer.
1) Is it possible to connect AVDD and VREF to the same power supply IC (using LDO) output 3.0V?
2) Do you know the current consumption of the digital part…
Part Number: ADS8866 Other Parts Discussed in Thread: OPA836
Hi Experts,
Our customer is interested in using the A/D converter. He has a question regarding its data spec documentation. On page 29, figure 53, there is a typical application Q Circuit for…
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8699 , Howdy!
I need to use industrial sensor for position sensing. It has 0 - 2.5V analog output. I was looking for some simple ADC capable of following parameters to digitalize the signal:
Vin =…
Part Number: ADS8866 Hi Team,
Can a single buffer be used to input a +3.3V reference to multiple number of AD8866s, three, running at a 100-kSPS rate?
Thank you.
-Mark
Part Number: REF6050 Other Parts Discussed in Thread: ADS8866 , REF5050 , TIPD211 , ADS8900B , OPA836 I'm hoping to use two daisy-chains of ADS8866 ICs in a multichannel simultaneous sampling system running at 50kHz. I currently have over twenty ADCs in the…