Part Number: ADS8866 Hi Team,
Can a single buffer be used to input a +3.3V reference to multiple number of AD8866s, three, running at a 100-kSPS rate?
Thank you.
-Mark
Part Number: ADS8866 Not sure if I have the latest datasheet, but I was wondering if the absolute maximum tolerated voltage at AVDD/DVDD power pins are still 4V? I run into a safety margin problem if applying 3.3V to these power pins with 10% derating…
Part Number: ADS8866 Other Parts Discussed in Thread: OPA836
Hi Experts,
Our customer is interested in using the A/D converter. He has a question regarding its data spec documentation. On page 29, figure 53, there is a typical application Q Circuit…
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8699 , Howdy!
I need to use industrial sensor for position sensing. It has 0 - 2.5V analog output. I was looking for some simple ADC capable of following parameters to digitalize the signal: …
Part Number: ADS8866 Other Parts Discussed in Thread: REF35 , , OPA333 , REF3330 Hi -
I am designing with the ADS8866 for a low power application. The TI REF35 looks like it would be the lowest power voltage reference to use.
I noticed in the ADS8866…
Part Number: ADS8866ADS8866 datasheet only specifies the max. operating ambient temperature Ta, but not the max. Junction Temperature Tj.
What is the max. permissive junction Temperature Tj of this part?
Part Number: ADS8866ADS8866 datasheet only specifies the max. operating ambient temperature Ta, but not the max. Junction Temperature Tj.
What is the max. permissive junction Temperature Tj of this part?
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8860 Dear Expert
We found that Pin 7 & Pin 8 data and clock output ringing . Could u give some advice about how to eliminate this ringing.
1.Pin 7 data waveform
2. pin8 clock waveform…
Part Number: REF6050 Other Parts Discussed in Thread: ADS8866 , TIPD211 , ADS8900B , REF50 , OPA836 , REF60 I'm hoping to use two daisy-chains of ADS8866 ICs in a multichannel simultaneous sampling system running at 50kHz. I currently have over twenty…
Hello Jacking,
The above waveforms show that MOSI is changing.
1. Is this connected to pin 9 (DIN) of the ADS8866? 2. Or, is DIN always connected to DVDD (high) as shown in the schematic?
The above waveforms show the device working correctly. Can…