Part Number: ADS8866 Other Parts Discussed in Thread: TIDA-01469 Tool/software: Code Composer Studio Hi,
I want to get a program about data transmission between ADS8866 and MSP_EXP430FR2311 via SPI protocol. The MCU (MSPFR2311) just need readout the…
Part Number: ADS8866
Hi,
I am planning to use ADS8866 to achieve local sampling close to the sensor. Using daisy chain seemed to guarantee that the conversion will start at the same time for all sensors.
Based on the manual, this is not sure. It is mentioned…
Part Number: ADS8866 Hi,
I want to use the ADS8866 with a reference voltage of 3.3V.
To get a good Resolution the expected voltage is in the range from 0V-3V.
If a fault happens the voltage can reach 5V. I protect the Inputs of the ADS8866 with a series…
Part Number: ADS8866 Other Parts Discussed in Thread: OPA333 , OPA836 , OPA320 Hi Friend:
Is there a Daisy chain connection AFE chip recommended? thank you
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8325 We use ADS8866 for measuring analogue signals. We use 3 wire mode. Supply voltage is 3V, supply voltage for reference is 3V switched (to reduce power consumption).
In most cases I get data…
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8325 , , TPS22917 We use ADS8866 for measuring analogue signals. We use 3 wire mode. Supply voltage is 3V, supply voltage for reference is 3V switched (to reduce power consumption). In most cases…
Part Number: ADS8866 Hello,
I have a problem with the nonlinearity of the ADS8866. In the picture bewlow you can see a Bending of the data (at around 17000 bits). I drive the ADC with a precise function generator, generating a triangle signal at around…
Part Number: ADS8866 Hi team
Does ADS8866 malfunction in the following sequence?
Power-Up : 30 msec after AVDD(3.3V) and DVDD(3.3V) rises, REF (5V) start rising.
Power-Down : After AVDD(3.3V) and DVDD(3.3V) decreases, REF(5V) gradually decreases over about…
Part Number: ADS8866 Hello,
What are the requirements on tquiet?
In the datasheet timing diagram (Figure 1) the end of tquiet is at the rising edge of CONVST but when is the start defined?
and what should be inactive during this time?
Many thanks!
…
Part Number: ADS8866 Other Parts Discussed in Thread: ADS8864 , 1:Hello, may I ask why Tconv in ADS8866 specification book is 500ns~ 8800ns time difference so big?And ADS8864 specification book Tconv can achieve 500ns to 1300 ns time difference is small…