Part Number: ADS8881 Other Parts Discussed in Thread: THS4551 Hi,
I understand that AVDD and DVDD can be driven independently, but are there any sequencing requirements at power-up or power-down? Or can AVDD and DVDD be enabled/disabled in any order…
Part Number: ADS8881 Tool/software: HI Sir
I use the fpga to reading the ADS8881, only can achieve 800k, Target is 1M
Could you provide the figure chart between ADC & FPGA Public board, and run 1M speed
thanks
Part Number: ADS8881 Hello,
One customer from NI EMERSON has a question about ADS8881. Please help to analyze:
【I am designing a data acquisition system base on ADS8881 to capture a sine wave signal from 0 ~100kHz(differential signal), my signal source…
Part Number: ADS8881 Other Parts Discussed in Thread: ADS8900B Tool/software: Dear team,
Currently, My customer are using LTC2328-18 for their application.
To replace this device, I found ADS8881 with similar function but this device is unipolar input…
Part Number: ADS8881 Hello, Few days back I got an ADC from TI as sample. The ADS8881. Since my application is very simple, I stick on to 3-wire CS mode, without busy indicator.
The connection is like this:
1. SDI connected to VCC through a 10K resistor…
Part Number: ADS8881 Other Parts Discussed in Thread: SN74LVC1T45 Hello
What is the recommended solution to drive 10 CONVST signals to get synchronous conversion on the 10 channels if I have 10 ADS8881?
Thanks
Yves
Part Number: ADS8881 Other Parts Discussed in Thread: ADS8883 the ADS8881 has different modes. i wanted to use the "10.4.2.1 Daisy-Chain Mode Without a Busy Indicator" because it seems to be the easiest if You only want to connect one device per SPi-interface…
Part Number: ADS8881 Other Parts Discussed in Thread: OPA2330
Hello, I encountered two problems when I using ADS8881 to have a test
1 ADS8881 datasheet have a measurement for ENOB(DC) as the following displays(Page 39), how to measure it actually…
Part Number: ADS8881 Hi Sirs, My customer failed to bring up the ADS8881 EVM GUI with the following error message. Would you pls provide tips to solve it? Thanks a lot Wayne Chen 07/19/2018