Part Number: ADS8881 Other Parts Discussed in Thread: ADCPRO Dear, Support Team. My customer is going to evaluate ADS 8881 EVM. The customer wants to simultaneously measure voltage and current using two ADS8881 EVM. Is it possible to start conversion of…
Part Number: ADS8881
Hi,
I'm interfacing the ADS8881 with Altera DE1 FPGA board. The sampling rate is around 200ksps.
The ADC output has weird behaviors. When sampling a DC input, the ADC output is correct for some samples and then becomes another…
Part Number: ADS8883 Other Parts Discussed in Thread: ADS8881 , , ADS8885 , ADS8887 , ADS8860 What is the maximum input current through the ESD input protection diodes? What would be a safe value for continuous situation?
Note: "ADS888x", I mean ADS8881,…
Part Number: ADS8881EVMV2-PDK Other Parts Discussed in Thread: TINA-TI , ADS8881 Tool/software: TINA-TI or Spice Models Hi, I'm learning the input driver design and reference driver design of SAR ADC.
Can TINA-simulation reflect the actual situation…
Part Number: ADS8910B Other Parts Discussed in Thread: ADS9110 , ADS8881 Hi Team,
Is there an alternative part for the ADS8910BRGER? Preferably P2P.
I found one is ADS9110 , I'm not sure if it's suitable.
Thank you.
Darren
Part Number: ADS8881 Hello,
In the ADS8881 datasheet, there is the spec of tconv (min) as 500ns.
I think that only the provision of max is sufficient, why does TI specify min of conversion time? Best Regards, Ryuji
Part Number: ADS8881 Hi team,
My customer is interested in ADS8881 and they're curious what kind of test bench (Differential Voltage Source) could help them to evaluate the chip's performance accurately.
Could you kindly share which instrument…
Part Number: AFE58JD28 Other Parts Discussed in Thread: ADS8881 , THS4130 Dear team,
I am using the AFE58JD28 with the THS4130 driving ADS8881 for the CW mode.
1. However, except for the noise requirement, I don't know how to evaluate the GBW requirement…
Part Number: ADS8881EVM-PDK Hi,
I have an issue driving the inputs of the EVM properly. The front end THS4551 seems to have a very low input impedance (<10k) making it hard to drive with normal opamps.
For example I am using it in an optical acquisition…
Other Parts Discussed in Thread: ADS8885 , ADS8881 Hello,
We're evaluating the ADS8881 on the ADS8885 EVM without the MMB0. We've evaluated the device in both the four wire configuration and three wire configuration, and in both see unexpected output…