Part Number: ADS8883 Tool/software: Hello,
When we were using ADS8883, we found that the input analog quantity exceeded the limit and the output quantity overflowed, causing a problem with the output complement code (previously we thought that the overflow…
Part Number: ADS8883 Hi,
Since many ARM based controllers (eg: STM32L4 series) allow setting the SPI Data Size (DS) from any value between 4 and 16 bits, how do we transfer 18 bit values from the ADC to the microcontroller?
More specifically,…
Part Number: ADS8883 Other Parts Discussed in Thread: ADS8881 , , ADS8885 , ADS8887 , ADS8860 What is the maximum input current through the ESD input protection diodes? What would be a safe value for continuous situation?
Note: "ADS888x", I mean ADS8881…
Part Number: TPS22991 Other Parts Discussed in Thread: ADS8883 , I am planning to use TPS22991 to control power to a wheatstone bridge type sensing element which has a bridge resistance of approximately 5kOhms. The aim is to low power operating by only…
Part Number: DAC7716 Other Parts Discussed in Thread: DCP020515D , , ADS8883 , OPA4990 , DAC8234 , DAC8734 , PGA855
Tool/software:
Hello,
I am using two DAC7716 on our board and they are being powered by a DCP020515D part. Through testing at around…
Hi Nic, The ADS8685 is a nice part, but - there is a PGA on the input that limits the bandwidth to about 15kHz. The devices that we have which are specifically designed for audio, don't usually work well outside the human auditory range. The ADS8883 might…
Hi Stefan
In order to meet your requirements, you can consider the following single channel devices from the SAR ADC portfolio:
1) ADS8881 - 18bit, 1Msps, SPI, Fully Diff
2) ADS8883 - 18bit, 680ksps, SPI, Fully Diff
3) ADS8885 - 18bit, 400ksps,…