Other Parts Discussed in Thread: ADS900 Dear friends,
I bought some ADS900 A/D converters some time ago, and found that some of them could be defected. The way I test them is to measure the resistance between pins 13, 14, 19 and 20. M y question is…
Other Parts Discussed in Thread: ADS900 , THS4509 Hi,
I want to use the CM port of ADS900 (1.5V) to bias 3 single-supply amplifiers at the same time. Is there any problem with that?
Thank you very much for your kind reply!
Lingli
Part Number: CC2642R Other Parts Discussed in Thread: ADS900 Tool/software: Code Composer Studio MCU ==> CC2642R BT5.0 ADC ==> TI ADS900 10 bit ADC with parallel interface
Our application requires very fast data transfer from the external ADS900 . There…
Hi Ilich,
We do not have experience with interfacing ADCs to the uPP port of these processors. You may need to check in the appropriate forum for those devices to figure out what interface may work.
You can look at an ADC like ADS900 that has a parallel…
Yury,
Are you sure you have the correct part?
Texas Instruments has the ADS900, ADS901, ADS930, and ADS931. However there is a part called the ADS-932 made by Datel and you can find their datasheet here:
www.datel.com/.../ads932.pdf
Joseph…
Hi Ronnie
A product like the ADS900 and the DEM-ADS9xxE evaluation board is pretty close to what you are looking for.
http://www.ti.com/product/ads900
http://www.ti.com/tool/dem-ads9xxe
I hope this is helpful.
Best regards,
Jim B
Hi, Richard,
Thanks a lot for your reply!
Here is more information for you about this issue:
The board we are using is designed according to previous project in which we were using an ADS900. The only difference between
these two boards are…
Other Parts Discussed in Thread: ADS6425 , ADS900 , ADS800 , ADS5294 , ADS5263 Hi,
I have look at the datasheet of ADS644 and ADS6425 to check if it is possible to used either in the single-input configuration. But did not find any information on single…
Hi,
On that generation of devices, the digital data was generally expected to be clocked into an FPGA or ASIC using a copy of the same sample clock that goes to the ADC itself. I don't see an EVM specific for the ADS809, but EVMs for similar devices…
Hi,
We do offer an evaluation board for the ADS930, as may be seen at http://focus.ti.com/docs/toolsw/folders/print/dem-ads9xxe.html
This is one of our older EVMs and comes with a printed copy of a User Manual in the box, but the User Guide has…