Part Number: TSWDC155EVM Other Parts Discussed in Thread: ADS9817EVM , , ADS9817 Tool/software: Hi team,
Our customer is using TSWDC155EVM to evaluate ADS9817EVM for system performance.
The EVMs work well with the GUI, but when customer use JTAG or…
Part Number: ADS9817EVM Other Parts Discussed in Thread: TSWDC155EVM , , ADS9817 Tool/software: I am conducting an operation check with a combination of ADS9817EVM and TSWDC155EVM.
A square wave with an amplitude of 5Vpp and 1kHz is input to AIN1P.…
Part Number: AFE58JD16 Other Parts Discussed in Thread: ADS9817 Tool/software: Hi E2E Forum,
We're wondering if the AFE58JD16 supports DC coupled input. It appears perfect for our use case except for the AC coupled inputs. Is it possible to use this…
Other Parts Discussed in Thread: ADS9813 , ADS9811 , ADS9817 I would like to get the finalized datasheet for ADS9813 / ADS9811, as the prelim datasheet didnt show up the package/mechanical/dimension information. Understand that this is a new product,…
Hello Zoey,
We have recently released the ADS9817 which fulfills the above requirements. It is only 8 channels though so and external multiplexor, or two ADCs may have to be used to achieve the 16-channel requirement.
Which customer is this for and…
Hi Dino,
The ADS8881 and ADS8900B are the most similar to the LTC device. However, they are both unipolar as you have mentioned. This E2E post tags an app note that may be referred to for bipolar to unipolar conversions . ADS8900B has very low noise…
Hi Tess - how many channels are required for this application? We have an 8-channel device in preview now which includes a similar integrated AFE with selectable low-pass filter bandwidth (21 kHz and 400 kHz). This device has two ADC cores, each with…