Other Parts Discussed in Thread: AFE1256 Dears, i am developing a large number of channel x-ray detector for dosimetry and I would like to use the AFE1256.
The device comes with a package type COF which is a standard FPC-to-PCB connector (0.5mm pitch…
Hi Team,
I have two question from my customer.
May I know what different about the package AFE1256GBTD and AFE1256TDS? Do you have comparesion table?
They want to design a FPD 10” application. They want to know how many pcs of AFE1256s on…
Hi Xurong,
The AFE1256 is intended to be directly connected to the sensor via ACF/thermal bonding. Usually, connectors with such fine pitch are not available or not useful for production.
One option is to use AFE0064, that is TQFP package. however…
Part Number: AFE0064 Other Parts Discussed in Thread: AFE1256 , AFE2256 , DDC264 Hi
I'm looking for an analog front-end IC with an input charge range of 0.75pC to 10.5pC.
I was wondering if the AFE0064 would be suitable for reading the continuous…
Like all our parts, the AFE0064 was designed with specifications given by our experienced customers. So you can be assured the statements in the datasheet is true. We won't be able to consult you on how to build the system. Any questions on how to use…