Part Number: ADS1293 Other Parts Discussed in Thread: AFE4400 , , AFE4900 , CDCE913 Hello,
I have been developing a system that can record ECG and PPG simultaneously.
I have had success in getting data from both.
I have attached the images below in a zip…
Part Number: AFE4400 1.The configuration frequency of the official network code is 100HZ. If the frequency is changed, the macro (#define PRF 100) value needs to be changed, and whether the registers(0x05 and 0x15) need to match according to the frequency…
Part Number: AFE4400 Hello,
I'm currently developing something using AFE4400.
I found that when normally running, the PD_ALM and LED_ALM Pins are always 0v even when I unplug the SpO2 cable.
I tried to set CONTROL0 Reg to enable Diagnostic Mode…
Hi Suhas,
You can read the status of diagnostics by reading the DIAG register (Addr. 0x30).
Here is the suggested sequence for testing diagnostics completely through firmware.
1. Enable Diagnostics by writing 0x40 to CONTROL0 register (addr. 0x0)
2…
Part Number: AFE4400 Hi Team
We have to make one medical wearable having following sensors requirement
1) Skin Temperature
2) Galvanic skin response
3) Accelerometer
4) Ambient air temperature
5) Heart rate
6) Respiration rate
7) SPO…
Part Number: AFE4420 I would like use AFE44xx AFE for new design of patient monitoring system. Could anybody share with me TDS of this product.
My requirements 4LEDs and 2PHD plus analog input 0-150 mV expected (but may be as well converted to current…
Part Number: AFE4400 In the calibration of our custom afe4400 board using " Fluke ProSim SPOT Light SpO2 Pulse Oximeter Analyzer".
The afe4400 register configuration is same as of afe4400spo2_evm. Using this same configuration(Led1,2 = 4mA)…
Part Number: AFE4400
The datasheet suggest that the number of samples used per conversion phase is preset to 2.
Is there a way to change this? If so, what register settings would I need to change?
I have a customer sampling at 125Hz with a 25% duty cycle…
Part Number: AFE4400
Is Thermal ground pin available on AFE4400. The EVM Board shows pin 41 as a EP Pin, connected to ground but the datasheet of AFE4400 doesnot indicate pin 41. Kindly request your clarification
Thank you