Part Number: AFE4404 Tool/software: Dear Sirs.
I use AFE4404 in low power device. I need to reduce power consumption of LEDs.
Pulse repetition factor is 10ms
Today I switch LED on for 230us and wait 70us between switching the LED On and starting…
Part Number: AFE4404 Tool/software: Hi,
I am trying to reads data from multiple registers (from 2Ah to 2Fh) sequentially.
I used nrf52840 to read, and I used i2c_burst_read_dt() function which can read multiple bytes from an internal address of an…
Part Number: AFE4404 Hi.
I was changing Hz using AFE4404 EVM.
I want to freely change the Hz in code just like when I put the desired Hz into Pulse Repetition in AFE4404 EVM, the 0x00 to 0x1E register value changes.
So I'm curious about the formula…
Part Number: AFE4404 Tool/software: We use AFE4404 sensors in our smartwatches, and have two questions.
First, Is the algorithm AFE4404 sensors estimating SpO2 based on the paper "Source–Detector Spectral Pairing-Related Inaccuracies in Pulse Oximetry…
Part Number: AFE4404 Hi.
I have a question while I was picking ppg with afe4404.
I understand OFFDAC, Gain.
But I don't know the function of the CF.
Thank you.
Part Number: AFE4404 Hi.
I was looking at the code Calibration_AFE4404.c initCalibrationRoutine() and left a question.
Can you tell me why the formula below came out?
Why do you save it in four variables using hysteresis percent: LOW_THR_HYS_LOW…
Part Number: AFE4404 Hello,
I am trying to increase AFE4404 data reporting frequency to around 60 HZ using the following public arduino code.
https://github.com/rakshithbk/AFE4404-Library/blob/master/AFE_Connect/AFE_connect.cpp
But however I tried…
Part Number: AFE4404 I have a special test mode that is need. It requires that all three LEDs be on at the same time for most all of the Repetition Interval.
The "normal" operational settings are for 100Hz at 1% duty cycle, with typical sequential sampling…
Part Number: AFE4404 Hi.
I am extracting PPG data using AFE4404.
I want to get pulse, spo2, and blood pressure with PPG data, is there a guideline or code provided by TI?
Thank you.
Part Number: AFE4404
Hello TI experts,
My customer considers AFE4404 for their new product, wearable smart wrist band.
and they want to know the answers about 2 questions below.
1. they will use photo sensor which is same as AFE4404 EVM. (NJL5513R…