Part Number: AFE4404EVM I have buy the AFE4404EVM Broad, and create the platform.
But the hardware i have try the use the oscilloscope measure the signal.
But the TX1~3、INM and INP I can not check the signal is true or false, so the compane can give me…
Part Number: AFE4404EVM Other Parts Discussed in Thread: AFE4404 Hi Guys,
I installed and carefully assembled the the hardware boards (sensor and micro-controller). After going through the procedure to disable signature enforcement given here earlier,…
Part Number: AFE4404EVM Other Parts Discussed in Thread: AFE4404 I am trying to replicate the AFE4404 EVM GUI and plot the waveform. Below is a waveform from the GUI.
I know the data read from NJL5513R sensor is a 3-byte data, e.g. 01BCE1 (hex), but I…
Part Number: AFE4404EVM
Hello,
If the AFE is placed on the same PCB as that of sensor and instead there is a cable between AFE & MCU, then can I avoid placing the BAV99W diodes between sensor & AFE?
Thank you.
Part Number: AFE4404EVM Other Parts Discussed in Thread: MSP430F5529 , , AFE4404 Hello,
I am trying to run the AFE4404EVM firmware on an MSP430F5529 launchpad http://www.ti.com/tool/MSP-EXP430F5529LP . This is the same chip that is used on the AFE4404EVM…
Part Number: AFE4404EVM Other Parts Discussed in Thread: AFE4404 The AFE4404evm Guide mentions that there EVM has SFH7050 and BMA280.
It says if to use SFH7050, R1, R3, R5, R7, and R9 should be installed. How?
Also, for BMA280 how to access its output…
Part Number: AFE4404EVM Dear TI
1. Why the EVM put an indutor(L1) on the analog input?
Will it not affect the frequency response?
2. The protection diodes(D3~D7) are for ESD or the feedback current of the LED
Part Number: AFE4404EVM Hello,
I have been using AFE4404EVM on a windows PC. I now want to use it with a macbook. Is it possible? The guide I have is based on windows (i.e. the GUI and the drivers etc.)
What is the other alternatives to communicate with…
Part Number: AFE4404EVM HI,
AFE4404EVM gives raw data, is there product / module that give actual reading on HR and SPO2 level, not just raw data?
Thanks