Part Number: AFE4490 Tool/software: Hi,
We are using AFE4490 in one of our designs. We are using a push pull configuration with common anode connection for the LED. We are facing problems for detecting LED shorts. Mainly the LED which is connected between…
Part Number: AFE4490 Tool/software: I'm trying to build a device that acquires real time SpO2 value. Right now this is the working,
-Continuously acquire ambient and normal Red and IR values over a period of 2 seconds using DMA -Every 3rd cycle, acquisition…
Part Number: AFE4490 Tool/software: SPI readback is returning zero for ambient canceled red and infrared data after the AFE runs for around twenty minutes.
Part Number: AFE4490 Hello, I have a question about the bypass mode. I see that bypass is suitable for bypassing normal procedures. If I don’t need it, can I connect it empty. Below is my circuit diagram,Could you please check it out for me?
Part Number: AFE4490 Tool/software: Hi TI's experts,
I am new to AFE4490. While reading its datasheet, I am little confused by the pin usage of SCLK and related read/write mode.
On the datasheet(SBAS602H –DECEMBER 2012–REVISED OCTOBER 2014), P52,…
Part Number: AFE4490 Tool/software: Hi Ti experts,
During parameter tuning, I swept the AMBDAC of its allowed values while kept rest register values unchanged.
When the AMBDAC value equals 3μA, both the IR current and the RED current exceed 1.2V(after…
Part Number: AFE4490
Tool/software:
Is the default or factory value 0000?
Or is it the Reset Value = **** part of the datasheet? please tell me. By the way, with the settings in the datasheet If I accidentally write 1 in a place like the one where…
Part Number: AFE4490 Dear Sir/Madam,
I purchased AFE4490SPO2EVM and tested its SNR. I have questions about this AFE's SNR performance.
I was looking for the SNR measurements in the datasheet, and it seems that SNR was presented as noise-free bits…
Part Number: AFE4490 Hi,
I'm KH and I wondering AFE4490 ADC measuring voltage range.
By datasheet of AFE4490, LED1 and LED2 sample range is from +/- 1.2V.
What I wonder is why from -1.2V to 0V are needed to ADC measure.
Thank you in advance…
Part Number: AFE4490 Hello TI team,
We are currently developing an SpO2 device using the AFE4490 with an STM32 MCU. We have conducted tests using a simulator and a reference SpO2 machine.
During our tests, we observed discrepancies in the data acquisition…