Part Number: AFE53004W
I finally got a setup with a modified DAC6300WCSP-EVM with the AFE53004W installed. The setup in general is working as the board responds to the microcontroller and the data flow via 4-wire SPI working as expected. Yet, the ADC…
Part Number: AFE53004W
I need some additional information on how to use the ADE53004W blocks in ADC mode with respect to HiZ/finite impedance input:
The datasheet states, that block 3 and any additional block that is to be used as ADC must be set…
Part Number: AFE53004W Hi team,
Customer get one inquiry regarding the SDA, SCL pin.
The pin table mention, it could power up before VDD. While the max rating shows it max is VDD + 0.3V, which mean it can't support SCL, SDA and other digital input…
Part Number: AFE53004W Other Parts Discussed in Thread: DAC63004WCSP-EVM
Hi,
more questions popped up while working the driver for the device since my previous post, most of which are not related to the ADC, so i decided to put them in a separate…