Part Number: AFE5401-Q1 Dear,
The customer wants to use AFE5401 ADC for their new project, with STM32 processor and plans to use its PSSI (Parallel Synchronous Target Interface) parallel interface to receive ADC data, But the ADC has two synchronization…
Part Number: AFE5401-Q1 Tool/software: Is the GUI software of AFE5401 only for EVM? Do I not have a development board to use it? Why is there no interface when I install the software of SLAC810, and there is no option of AFE5401 in the High Speed Data…
Part Number: AFE5401-Q1 Tool/software: Hi,we are selecting two AFE5401 chips for sampling. The sampled data is output as CMOS data, and then the data is processed by the TDA3. Do we need a CPLD for data conversion between them, or can we directly connect…
Part Number: AFE5401-Q1 Tool/software: The clkin provided by AFE5401 is 50MHz. I carried out a 2-frequency division internally according to the manual. Then it was set to 4-channel sampling, but the output clock dclk was only 50MHz. Could you please take…
Part Number: AFE5401-Q1 Tool/software: The afe5401 official website development board schematic diagram has a DC bias connected, but ours is not. Can it be used normally? Will it have an impact on which parameters?
Part Number: AFE5401-Q1 Tool/software: Hi,
How should the AFE5401 be configured so that there are few cycles delay between DSYNC1 and DSYNC2 after the TRIG trigger? This is necessary because the VIP input port of the TDA3x requires a certain time difference…
Part Number: AFE5401-Q1 Other Parts Discussed in Thread: TMS320F28386D
hi. I have a question about configuration for using external adc such as AFE5401 in dsp.
I wonder how CLKIN and DCLK should be connected to dsp.
I'm using TMS320F28386D as a…
Part Number: AFE5401-Q1 Tool/software: HI,
Please tell me about unused PINs. Normally, I think there is no problem with input PINs being pulled up or down and outputs being OPEN.
Are there any recommended methods for handling unused pins for the pins…
Part Number: AFE5401-Q1 Tool/software: Hello,
We encounter an issue where while the unit is in operation, the auxiliary channel 1 would start outputting zero (not exactly zero, but close to zero). Power cycling the AFE5401-Q1 will clear the issue and…
Part Number: AFE5401-Q1 hi. I have a question about DCLK of AFE5401.
Is DCLK is unconditionally output when a clock is input to the chip?
I'm inputting 25 MHz clock into the chip, but dclk is outputting 3.3v and the waveform doesn't occur.
I would…