Part Number: AFE5803 Hello, I am looking at using the AFE5803 in an application where the sensors are some distance from the readout electronics and would like to route the sensor signals differentially.
In looking at the ADF5803 datasheet section concerning…
Part Number: AFE5803 Hello, Support Team, I want to use one pair PLL clock of FPGA to drive 4 piece AFE5803. But there is no information of suck current in AFE5803 datasheet. Is there any risk if I do it? should I add a clock driver IC for 4 piece AFE5803…
Part Number: AFE5803 According to page 46 of AFE5803 datasheet, it state that “The VCA wake-up response is typically about 2
μs or 1% of the power down duration whichever is larger. The longest wake-up time depends on the capacitors
connected…
Other Parts Discussed in Thread: AFE5803 Hi,
In AFE5803 datasheet (Page 48) LVDS trace difference length is given as <3.81mm. Am I correct in thinking that this contraint is that between LVDS pairs, or is it between traces in each pair, or both?
Sa…
Other Parts Discussed in Thread: AFE5803AFE5803 the digital input specs ( vin hi and lo ) look to be a type since they are powered by DVDD which is 1.8V
HI,
I am planning to buy an ultrasound front end solution.
I have read the TSW1400 documentation, and it supports external trigger and capture option.
Question 1.
If I use an ADC AFE58~ serise with TSW1400, is it possible to save more than 20khz repitition…
Other Parts Discussed in Thread: AFE5803EVM , AFE5803 I can't get past page 9 of SLOU332B - AFE5803EVM Evaluation Module User's Guide
The error message I get from HSDC Pro (v4.10) is "Check if USER_LED2 is OFF" - it is ON and "Clock from ADC EVM…
Other Parts Discussed in Thread: AFE5803 , CDCM7005 Hi,
I'm using AFE5803 evm for my school project.
I set up my evaluation board just as mentioned on page 3/4 of the 5803evm guide, but with the following two differences:
I connect Pin 1&2 of …
Other Parts Discussed in Thread: AFE5803 Hi,
I would like to ask you a question about PGA gain as below.
My customer has been evaluating AFE5803 and recently has a problem with PGA gain 30dB.
They observed PGA gain 24dB correctly working but about 30dB…