Part Number: TSW1400EVM I have been using High Speed Data Converter Pro with a TSW1400 and AFE5803EVM to capture data. I have been using an external 10MHz clock from the TX7316EVM CLK_10M_OUT SMA connector. In the AFE5803EVM GUI, I leave the clock set…
Part Number: AFE5803EVM Purchased a AFE5803EVM. Supplied 5V, -5V and COM. Board powers up per the document but after a short time the 5V drops to 2.5V and the two red LEDS go out. I don't know whats going one here.
Part Number: AFE5803 Other Parts Discussed in Thread: SN74AUP1T04 , , ISO7240M According to Table 12 of the AFE5803 datasheet, the ADC SPI output is powered from DVDD (1.8V). Following Figure 58, there is also a note saying that the "SN74AUP1T04 can be…
Other Parts Discussed in Thread: AFE5803EVM Hello,
Is it possible to install the AFE5803EVM GUI on Windows 10? I installed, restarted, and launched the GUI, and I got the following error message:
Thanks for your help.
Paul Hultz
Other Parts Discussed in Thread: AFE5803EVM , ADS5474EVM , ADS5474 , AFE5803 Hello,
We are using AFE5803EVM as well as ADS5474EVM and TSW1400 for data collection and export. Here we meet 2 questions:
Firstly, is the Quartus project in the TI website( www.ti…
Part Number: TSW1400EVM
Hello, I have downloaded the firmware source of TSW1400EVM from www.ti.com/.../tsw1400evm , then I have tried the code with AFE5803EVM using the original "defines.vh" and it works. But when I switched to ADS5474EVM with INTERFACE_ID…
Other Parts Discussed in Thread: AFE5803EVM , AFE5803 I can't get past page 9 of SLOU332B - AFE5803EVM Evaluation Module User's Guide
The error message I get from HSDC Pro (v4.10) is "Check if USER_LED2 is OFF" - it is ON and "Clock from ADC EVM…
Other Parts Discussed in Thread: AFE5803 , AFE5803EVM , HSMC-ADC-BRIDGE I am designing a data acquisition system which uses TI AFE5803 with LVDS connection to Altera CycloneV FPGA.
For the development project, we are using AFE5803EVM with an HSMC-ADC-BRIDGE…
Other Parts Discussed in Thread: AFE5803EVM I have been looking at LM965XX chip set, but still have questions on best way to evaluate them in a system (TX-SDK-V2, LM96511EVK, AFE5803EVM, …..).
Is there a recommended platform to start with?
-Jad…