Hi,Haiteng,
the output FCLK of my AFE5805 don't have frequency output, I doubt with my configuration data which may be wrong,could you share the configuration data with me?
Thanks!
chao zhu
Other Parts Discussed in Thread: AFE5805 , AFE5805EVM Hello,
LCLK frequency should be 6x bigger than FCLK/ ADCLK when register 46 config to DDR, and 12x bigger when config to SDR. That is correct, right?
But in my tests LCLK is just 3x bigger in DDR configuration…
Hi Vincent
One reason which I think it is the AFE5805 is not coming in is because you might not have installed the GUI for AFE5805.
Because when you install device GUI, some files get copied in the HSDC libraries and the list gets updated. And then you…
Other Parts Discussed in Thread: AFE5805 I need some information about TSW1400 to see if I should buy it to my project.
I have AFE5805 and a TSW1250 but I need get the 8ch simultaneously, I will need a diferent adapter or TSW1250-AFE58XX works for it?
…
Other Parts Discussed in Thread: AFE5805 , THS4130 Hi all,
I have an application using an AFE5805 in a multibeam sonar, and have a query concerning the voltage control signals used for gain control.
The gain control signal are presented as a differential…
Hi Suresh,
1) The TX_SDK_V1 and TX_SDK_V2 are the only EVMs for TI's HV pulser.
2) TI internal has power module with power on/off sequence built in for the above mention EVMs. However, it's not for sale. We are trying to put the power module schematic…
Other Parts Discussed in Thread: TX810 , AFE5805 , AFE5808A , TPS54060 , LM96570 , TPS54120 Hi, my name is Valeri.
TI offers a chipset for a portable ultrasound probe which consists of LM96550 - Tx pulser, LM 96570 - Tx beamformer, LM96530 - Tx/Rx switch and…
Other Parts Discussed in Thread: AFE5805 , AFE5805EVM Hi,
I am designing a ultrasound device now. In AFE5805 datasheet, it says that the pin VCA_CS# (H4) can be connected to pin RST(H5). Does this means these two pins can be connected directly? In AFE5805E…
Other Parts Discussed in Thread: AFE5805 Hi,
I do posses one AFE5805 EVM+TSW1250. I need to configure the AFE5805 through SPI interface for it to produce deserialization patterns and not through USB. Somebody please guide me to have the settings for EVM…