Other Parts Discussed in Thread: AFE5805 , AFE5808 Hi
I want to replace AFE5805 with AFE5808 in one of my project. What are all the things that i'll have to consider before proceeding???
Other Parts Discussed in Thread: AFE5805 I need to transfer data from 4 AFE5805 devices to a Laptop for an industrial ultrasound application. The data is filtered and oversampled resulting in 32 channels at 4 to 6 Msamples/sec for an aggregate date rate…
Other Parts Discussed in Thread: AFE5805 Hi all,
I'm having TSW1250 and AFE5805 EVM's with me. To get the deserialized output correctly on TSW1250 GUI I supply 3 data ( [0.1],[42,8081],[46,8208] ) to 3 registers as noted in the user guide in the AFE5805…
Do you use AFE5805 USB SPI. If yes in send these datas as given
Step 1: Address: 0
Data :1
Step 2: Address: 42
Data :8081
Step 3: Address: 46
Data :8208
Now i think your problem will be resolved...
Hi all...
I am working with TSW1250 and AFE 5805 boards. For controlling i have two GUI to interface with these two boards. Please somebody provide me the help documents for these GUI's.
i am not a expert on the signal convertion. however when i read the datasheet of the LVDS32. looks like it can only handle data rate up to 100M. this could be too low for AFE5805. since the output data rate is over 500Mhz. there may be some other coverters…
Other Parts Discussed in Thread: AFE5805 hai,
This is sivakumar , i am using AFE 5805 EVM board with FPGA desearializer board, i teseted deskew pattern and sync pattern of serializer(LVDS) it was working.but i want to check ADC i applied 250MV PP in…
Part Number: AFE5801 Other Parts Discussed in Thread: AFE5805 , hello,
Could anyone help with the details of the bridge board to be used between AFE5801 and TSW1405.
AFE5801 is not mentioned in the drop down in TSW1405 in HSDC pro. But AFE5805 is…
Hi Chen,
I have bought the TSW1495EVM and downloaded the software from TI website. However, when I connect with AFE5807EVM, I can not find this model in FPGA software, I can only find the AFE5805. What is the possible reason? Thanks
Best,
Guang
Chen,
There seems to have been a small mistake in the post. The board in use is the AFE5805, rather than the AFE5808 listed. This error in name was only made within this thread post, not in any of the previous working files selected. Are you able to provide…