Part Number: AFE5808 Other Parts Discussed in Thread: , AFE5807 , AFE5803 We are currently looking at temporarily replacing the AFE5808A with AFE5808 due to supply issues. One of the differences between the parts seems to be that it does not have the…
Part Number: AFE5808 Hello Guys,
Good day.
Our customer is currently working with an ultrasound system which uses AFE5808 circuit. As per their understanding, the ADC uses 1.5 V (REFP) as a positive reference and 0.5 V as the negative reference (REFM…
Part Number: AFE5808 DEARS.
We are testing with AFE5808/08A EVM.
I need a source file and a way to check the contents of the BIN file.
How can I check the initial register value of the AFE5808 / 08A EVM?
How can I check the changed setting values…
Part Number: AFE5808EVM Other Parts Discussed in Thread: AFE5808 Hi TI Expert,
I open this thread to ask you if there is any ".c" that contains the initialization (boot) programming of the AFE5808EVM board.
i.e., I want to do the same as the IT…
Part Number: AFE5808 Hello TI Experts,
I am using AFE5805A to do Ultrasonic analog front-end signal processing.
I find that the static noise between channels is quite different~
Test conditions:HDL6M05585 keeps the input state all the time,128 ultrasonic…
Part Number: AFE5808A hello, TI expert,
I have a question about the AFE5808A device, so I send an email.
I want to set the custom address to A33 in the AFE5808A.
Is the AFE5808A custom pattern setting correct as shown below?
12bti serialize…
Part Number: AFE5808 HI team,
Here is FAE in south China, my customer has some concern on the noise of CW doppler:
for input voltage noise, 1 channel is 0.8 while 8 channel is 0.33? why 8 channles has lower noise than 1 channel?
the same thing…
Part Number: AFE5807 Other Parts Discussed in Thread: AFE5808 , AFE5808A Hello,
My customer has a question about AFE5807 and AFE5808(A).
[Q]
Please tell me the difference between AFE5807 and AFE5808(A).
<My understanding>
* Analog Front-end…
Part Number: AFE5808 Other Parts Discussed in Thread: ADS8900B , TIDA-01351 , Hi Experts,
Our customer is using AFE5808A as the altrasonic AFE circuit referring to TIDA-01351 CW circuits, and they want to know if we have any example registers configurations…
Is there any update on this topic? We are trying to integrate AFE5808 and TSW1405.
We cannot find the device in drop down. It will be great if you can provide the ini file for the same. Also, what should we select in the "Download Firmware" section…