Part Number: TSW1400EVM Hi,
I'm currently using a TSW1400EVM to connect to AFE5808AEVM. After power up, the 5V input should draw around 0.37A. The only LED C87 is on. The power supply for AFE5808AEVM is providing +-5 volts and slightly over 0.7A. …
Part Number: TSW1405EVM We are trying to interface AFE5808AEVM with TSW1405EVM .
Older thread: https://e2e.ti.com/support/other_analog/imaging_afes/f/239/t/407866
As per both related devices section of TSW1405EVM, only ADS12* series products are mentioned…
Hi,
When you are using TSW1400EVM to capture AFE5808AEVM,
please make sure the P10 connector (on AFE5808AEVM) must be connected very tightly to TSW1400EVM.
Please also double check on AFE5808_08A User's Guide's Figure 1 on page 3,
since you are…
Part Number: AFE5808A Hi Team, The datasheet specifies the common voltage of the AFE5808A low noise amplifier to be 2.4V. However, our customer measured 2.25V on one channel using the AFE5808AEVM. Is this measured value from the expected characteristics? Can…
Hi,
The picture shown from the customer is not clear to us.
therefore, first, can the customer run the clock speed slowly
such as 40MSPS?
How the customer capture those data?
Do they use AFE5808AEVM and TSW1400EVM to capture these raw data?
Or they are…
Part Number: AFE5808A Other Parts Discussed in Thread: AFE5832 , , AFE5808 , AFE5816 ,
Hi,
I have seen that some datasheets from advanced ultrasound front-ends like the AFE5816 and AFE5832 specifies that INPx and INMx pins must be protected in the PCB layout…
Part Number: AFE5816 Other Parts Discussed in Thread: AFE5818EVM , AFE5808AEVM , AFE5809EVM , HSMC-ADC-BRIDGE , FMC-ADC-ADAPTER , AFE5818 , , AFE5809 , AFE5808A Hello,
My customer has a question.
[Background]
They would like to evaluate AFE58xxEVM by connecting…
Hello, Jim
When I disconnected the AFE5808AEVM from TSW1400EVM , After the AFE5808AEVM GUI has launched, LED41 and LED42 go off and the rest of the LEDS remain on. I wonder why we need the power supply of 3A. Is the current of the board working at…
Hi Henry,
How are you?
Using TSW1400EVM to capture LVDS output data from AFE5808/08AEVM,
Please take a look at the TI website User guides:
www.ti.com/.../afe5808aevm
we support the TSW1400 firmware for your TSW1400EVM.
TSW1400ADCDACFirmware-2.2-windows…
Hello Olu,
Thanks for the reply. It is unfortunate to hear that TSW1405EVM is no longer supported with AFE devices. We had bought the devices and have been using AFE5808AEVM for the last few months (with TI's support). Sadly, a power issue caused severe…