Part Number: AFE5816 Hi,
According to the AFE5816 datasheet, "the ramp, toggle and pseudo-random sequence (PRBS) test patterns can be reset or syncronized by providing a synchronization pulse on the TX_TRIG pin or by setting and resetting a specific…
Part Number: AFE5816 Other Parts Discussed in Thread: AFE5808A Hi,
It seems no data output format is specified in the datasheet. Are data in two-complement or offset-binary format? Other parts, like AFE5808A, allow the user to choose between both formats…
Part Number: AFE5816 I guess before we get to my question, what's up with the datasheet on the AFE5816? It's only a couple pages long, it used to be really long and detailed...I can't find the full datasheet anywhere. Please send that or update the website…
Part Number: AFE5816 Tool/software: Hi, everyone
Now i'm trying to test output of the AFE5816.
This is my register setting sequence for low-power mode operting.
01h / 0014h
41h / 8000h
42h / 8000h
41h / 0000h
42h / 0000h
03h / 2000h
…
Part Number: AFE5816 Hello, everyone
I am trying to verify the output from the AFE using a test pattern. I want to check the output data through ILA, and the clocks are as follows: ILA clock = 280MHz AFE input clock = 10MHz It is set to 14bit 1X serialization…
Part Number: AFE5816 I am trying to verify the output from the AFE using a test pattern. I want to check the output data through ILA, and the clocks are as follows: ILA clock = 280MHz AFE input clock = 10MHz It is set to 14bit 1X serialization.
In the…
Part Number: AFE5816 Is there a ChipID register (undocumented ??) that I can use to identify the chip by SPI read??. I couldn't find any chip id for this part in the datasheet.
Part Number: AFE5816 Hello TI Community,
I'm in the process of analyzing the AFE5816 chip for a planned design and have a few questions that I hope the community can help me with:
AC PERFORMANCE (Power) - AVDD_1P9 PSSR: I noticed in the AC PERFORMANCE…
Part Number: AFE5816 Hi,
My custom board uses AFE5816 for ADC.
Referrring to AFE5816 datasheet, I set my AFE5816 register with the initialization set up
This is my register setting sequence
0X01 - 0014
0X41 - 8000
0X42 - 8000
0X41 - 0000…