Part Number: AFE5816 Other Parts Discussed in Thread: AFE5818
Hi Team,
A customer can not use his company email to post query in E2E.
I help him to post this question.
↓
I have a question about power mode of ADC AFE5816AFE5816 have three power modes…
Part Number: AFE5816 Hi Team,
Our customer noticed that the output at LNA_INCM pin of AFE5816 is 0.6V instead of 1V as stated in the datasheet. What could have caused this lower output?
Thank you for your support!
Regards,
Danilo
Part Number: AFE5816 I need to DC-couple the input signal. Can I use the INMx as a reference to an external differential amplifier?
Or, can I simply drive the INMx with external reference DC signal?
Part Number: AFE5816EVM Other Parts Discussed in Thread: AFE5816 Hello,
I am following the SLOU429A guide to acquire data with the AFE5816 connected to the TSW1400. I've successfully followed all steps until section 4.2, but arriving in step 9 page 11 …
Part Number: AFE5816EVM Other Parts Discussed in Thread: AFE5816 , AFE58JD16EVM , Hello,
I've been examining the AFE5816 EVM Schematic and have a query about the interface designed for controlling TR_EN pins:
However, upon further inspection, I noticed…
Part Number: AFE5816 Hi Team,
Several questions about DTGC funciton of AFE5816/5832 from my customer for it i cannot find answer in datasheet. Could you please help me with it? All below questions are about "External Non-Uniform Mode"
1. When…
Part Number: AFE5816 Hi,
I could not find the info in the data sheet, but I guess it's 2's complement binary.
Assuming I have 12 bit selected, then it would be as follow:
MSB...LSB
011111111111 => +2047(max)
000000000000 => 0
111111111111…
Part Number: AFE5816 dear sir
l want to use afe5816 in my detection device. l want to know the delay time between the inter digital processor with lvds output pin ?
Part Number: AFE5816 Hi team,
I have a question about the operation of DTGC function of AFE5816: in "External Non-Uniform Mode", firstly the device is set TGC_UP_DN=0 to increase the gain up, then what will happen if TGC_UP_DN is set to '1' before the…
Part Number: AFE5816 Hi Team,
In datasheet of AFE5816 it mentioned "The phase reset from TX_TRIG can be disabled using MASK_TX_TRIG.". But i cannot find any pin or register bit named as "MASK_TX_TRIG".
Thank you,
John