Part Number: AFE5818 I configured the AFE5818 to test mode so that D1~D16 and FCLK alternate output 01, but in the waveform captured by the ILA, FCLK and D6/8/9/12 are always 1. I want to know what is causing this?
Part Number: AFE5818 I want to know the cause of the waveform anomaly and whether my register configuration is correct. The registers configured for the AFE5818 are: 0x00 0x0001 0x01 0x0014 0x03 0x2000 0x04 0x0011 0xC3 0x0050 0xC4 0x5000
Part Number: AFE5818
Dear TI Support Team,
We are using the AFE5818 in an ultrasound acquisition system and have encountered an occasional issue. We would appreciate your advice.
Issue Description: - The AFE5818 outputs LVDS data, which is converted…
Part Number: AFE5818
In my current project, I have been using the AFE5818 with its LVDS interface connected to FPGA banks operating at 2.5 V.
I am now planning a migration to a new FPGA, where – depending on the selected bank (HP or XP5IO) – the I…
Part Number: AFE5818 Hello,
Please provide information about AFE5818 ADC_CLK frequency range (min. / max.).
What is the input impedance of ADC_CLK ?
What should be the connection diagram for 50 Ohm single-ended clock? ADC_CLKM grounded and ADC_CLKP…
Part Number: AFE5818 What is SPI mode (CPOL/CPHA)?
The SPI timing diagram shown appears to start SCLK with the idle signal high (CPOL=1). I believe this is the source of the misunderstanding. Now that I look closer, when the SCLK signal immediately…
Part Number: AFE5818 Other Parts Discussed in Thread: AFE5808 Tool/software: I am reviewing a circuit to replace the previously used AFE5808 with the AFE5818.
The AFE5808 has a register that supports changing the ADC LVDS output to 16-bit. I would like…
Part Number: AFE5818EVM Other Parts Discussed in Thread: AFE5818 , DATACONVERTERPRO-SW Hello,
I am revitalizing an old test-setup that we developed with development board TSW1400EVM and the AFE5818AFE. In previous setup's we were able to use HSDC Pro…
Part Number: AFE5818 Tool/software: hello. I need a data sheet for the part numbers below. Part Number: AFE5818 I need a data sheet for design, so please provide me with detailed information. Ex) Pin map, detailed design