Part Number: AFE5818 Other Parts Discussed in Thread: AFE5808 Presentation for the problem for TI
We encounter a problem when sending a long burst of pulses on the AFE5818.
The problem is also the same with AFE5808.
In the drawing above, we see the…
Part Number: AFE5818 Dear Sir:
AFE5818 is about 6.5W when it is just powered on, when we adjust the external agc, the power consumption of the whole board will reach 13w. If the input afe5818 signal is disconnected, how to adjust the external agc, the…
Part Number: AFE5818EVM Other Parts Discussed in Thread: AFE5818 i use AFE5818 and TSW1400 when i want to capture signal there occured "
Read DDR to file
TIMED _ OUT _ ERROR Possible reasons for Time Out Error : 1.FPGA may be in reset . Please check…
Hi King,
Do you have access to EVM and GUI for AFE5818 and AFE5832? If you have installed these GUIs, then, the SPI config files for quick-start modes would be available in the below locations -
AFE5818 - C:\Program Files (x86)\Texas Instruments\HMC-DAQ…
Part Number: AFE5818 I had previously used this GUI with the AFE5818 and TSW1400 on an older laptop. But now I am having a problem. It shows error 1003 (please see the attached photo).
Part Number: AFE5818 Hello
our customer is using the LVDS interface to connect the AFE5818 with a FPGA. LDVS is not AC coupled.
In case the 1.8V Supply of the FPGA rises before the 1.8V_ DVDD-DIG of AFE5818 there is some backbiasing and you can measure…
Part Number: AFE5818 HI, AFE5818 engineers:
In my own AFE5818 hardware system, the AFE5818 samples at a rate of 12-bit and 80MHz. In actual use, errors will occur in the received echo data, as shown in the figure. These values should be close to 0, but…
Part Number: AFE5818 HI, AFE5818 engineers:
In my own AFE5818 hardware system, the AFE5818 samples at a rate of 12-bit and 80MHz. In Test Pattern Mode, no matter what data I set the AFE to send, the FPGA can receive the correct data, Which shows that…
Part Number: AFE58JD18EVM Other Parts Discussed in Thread: AFE5818 , TX75E16 Tool/software: I bought AFE5818 and TX75E16 from TI site last time.
TX75E16 is available in .brd(Allegro) PCB data from TI site, so there is no problem,
but AFE5818 cannot find…