Part Number: AFE5832 Other Parts Discussed in Thread: AFE5832AFE5832DEBUG2021_1103.docx
I have some problem about serdes AFE5832's lvds data.
1) Help to check the initialize procedure, what the right sequencing?
(1) Set a reset signal (period…
Part Number: AFE5832 Other Parts Discussed in Thread: , TX7332 The problem here occurs when we use AFE5832 to receive data. When we use test pattern, everything is ok and the received test data for all channels appear normal.
However, when we switch…
Part Number: AFE5832 Dear Sir :
We use AFE5832 to implement handheld ultrasound image system, but we face EMI issue now. Do you have any suggest to resolve EMI issue ?
The ADC sample frequency is 100Mhz, and EMI over spec. frequency is 300Mhz and…
Part Number: AFE5832 Hi Team,
One of my customers have question below:
About the "Figure 19. DTGC Mode Test: Waveform" of following user guide www.ti.com/.../slou489.pdf
I thought the output signal should be same as the input. Why is the waveform…
Part Number: AFE5832 Hi,
i have swaroop board with me and i have connected with phased array transducer. In GUI control im setting quick setup,i will click DUT HW Reset and click the Initialize device, then i will select the number transmitter and number…
I have solved the issue by setting pin K16 to High, Even though it says in the datasheet to keep it unconnected, which I presume is a typo. Many thanks,
Part Number: AFE5832 HI,
I have seen the application notes SBOA361.
I wonder if the board that is on demo is available for purchase? If not, is there any information or datasheet on that board design?
Thanks alot!
Yoon Hwee Leow