the AFE5832 itself is sufficent for gain and sonar settings. for sonar application, it is not necessary to use the JESD204B. LVDS is typically more than sufficient and cost effective.
for the TX, you can look into TX7316 and TX7332, but they are not designed…
Xiangang,
right now, we didn't verify this kind of approach. mulitple EVMs aligment will be an issue.
TSW1400 supports LVDS on a Non-FMC connector.
if you need more channels, can you look at AFE5832EVM? AFE5832+TX7332 should work nicely.
Thanks…
Part Number: AFE5808A Other Parts Discussed in Thread: AFE5832 , , AFE5808 , AFE5816 ,
Hi,
I have seen that some datasheets from advanced ultrasound front-ends like the AFE5816 and AFE5832 specifies that INPx and INMx pins must be protected in the PCB layout…
Part Number: TSW1400EVM
I`m trying to connect TSW1400EVM to AFE5832EVA.
I downloaded HSDC v5.0, but there is no firmware for AFE5832 in Select ADC.
Also, I can`t find AFE5832 GUI program. Other model`s GUI can be downloaded in TI homepage, but AFE5832…
Due to This research project , I must insert Analog LPF about 1Mhz BW .
I think to implement a new board which includes 32 LNAs + mixers for D. Convert + 32 Analog FILTERs + buffers and to connect it to the AFE5832 EVB using SMA cables .
My request …
The cause of the problem was that the unused LVDS inputs were not terminated correctly. This led to reflections and hence, the behavior I was describing. I solved the problem by forcing a 100-Ohm termination buffer for all channels. This is mentioned in…
Hi,
Here are the reply to your questions:
=============
The TSW1400EVM supports 16 LVDS lanes (This is a typo in the TSW1400EVM product folder).
32 channel data can be received with the combination of AFE5832EVM and TSW1400EVM.
AFE5832 packs the 32 channel…
Part Number: TSW1400EVM I'm using TSW1400EVM connecting with AFE5832EVM.
I already used their GUIs without automation dll successfully.
But when I try to run the MATLAB 64bit Automation example, I receive the error code like
>> Selecting ADC Device…
Hi,
Sorry for the TSW1400EVM typo.
The correct and more information for your questions as shown and listed below:
Thank you!
================
The TSW1400EVM supports 16 LVDS lanes (This is a typo in the TSW1400EVM product folder).
32 channel data can…
I'm currently using the version 4.70, and I know the latest one is 4.90 and I tried it. But 4.90 version said that AFE5832 EVM is not compatible with the version 4.90, so downgrade it to 4.70. The file is from the download section of AFE5832 datasheet…