Hi,
In the 'AFE5851EVM kit contents' (pg 4 of AFE5851EVM User Guide), it says that an AFE/TSW Adapter board is included. I hope that this will take care of the bridging issue (of connecting AFE5851EVM with ML605). But a confirmation will be appreciated…
Other Parts Discussed in Thread: AFE5851 , AFE5851EVM Richard,
Will this design be helpful in deserializing the output from AFE5851? Please do send the VHDL code for the deserializer to asasidharan@cdac.in.
I'm using Virtex-6 development board(ML605…
Other Parts Discussed in Thread: AFE5851 , AFE5851EVM We're planning to use AFE5851 in our project as the front-end data converter. We'll be using Virtex-6 for interfacing the AFE5851 (that is to configure it as well as to deserialise).
For testing…
I have an identical question concerning AFE5851. The DVDD = 1.8V, but the data sheet says on page 6: DIGITAL INPUTS High-level input voltage 1.4 3.6 V".
So how to drive the SPI with these chips? Are these inputs 1.8V or 3.3V - compliant? The output…