Part Number: AFE58JD48 Other Parts Discussed in Thread: TX08D , I recently requested the datasheets for TX08D and AFE58JD48. I received a follow-up email asking for more details about my application, and I responded with information about the project…
Part Number: AFE58JD48 Hi experts,
I want to configurate the analog TGC at 0.5 dB step. But how it can configurate through VCNTL? Can you please help provide some demo or guide documents? Thanks.
Part Number: AFE58JD48 Respected TI experts
We now tring AFE58JD48 in x80 mode with less highspeed GT link to xilinx FPGA xku5p devices,but the jesd204b link sometimes not bringup,so i using xilinx tools to scope the jesd204b phy output dat.I find that…
Part Number: AFE58JD48 Hello, I am using the Auto Offset Correction Mode of the AFE58JD48 chip. However, when I configure the parameters according to the register instructions in the datasheet, it has no effect, and the signal still deviates from the…
Part Number: AFE58JD48 When configuring the custom pattern to alternate between 16728 and –9981 (as shown in Figure 1), incorrect data is observed under certain conditions. Specifically, the received data becomes –9853 , which differs from the expected…
Part Number: AFE58JD48 Tool/software: Hello, I have a few questions for you:
Problem 1: reset to read the register, such as read 0xDF, read out as 0xC700, not the default value;
Problem 2: Operation register failure, such as 0x0040 written to 0xDF…
Part Number: AFE58JD48 Other Parts Discussed in Thread: TX7332 , Tool/software: Hello! Recently, we are developing an ultrasonic imaging system using TX7332 and AFE58JD48. There are several issues.
Firstly, what is the sampling start control signal…
Part Number: AFE58JD48 Tool/software: I hope to configure the AFE with FPGA and establish a high-speed interface using the JESD204B protocol (subclass 0/1/2). The AFE uses the 40x mode, and the correctness of SPI read and write has been verified.
…
Part Number: AFE58JD48 Tool/software: Hi TI experts,
The AFE58JD48 can pre-store up to four analog gains, i.e. TGC_PROFILE[3:0], which can be pin-selected to enable a certain TGC_PROFILE, how do I implement DTGC with the help of this function?
…
Part Number: AFE58JD48
Tool/software:
Hi TI experts,
I am planning to use one FPGA to communicate with two AFE58JD48 devices simultaneously. Both AFEs are working in 80x mode (4-lane mode). I would like to consider the two AFE58JD48 devices as…