Anush,
We do not have any verilog/VHDL code for AFE7225.
We use Altera Stratix IV FPGA to interface to this device. Follow the following site to find more information on how we interface our board to this FPGA. Maybe this information will be helpful…
Part Number: AFE7225 Other Parts Discussed in Thread: TRF370333 , THS3217 Hi team,
The DAC part of the AFE7225 is a current sink architecture. So a external pull up resistor is required for each DAC output pin.
The voltage divider resistors are to be selected…
Part Number: AFE7225 Hi
I am interested in designing a multi channel modem using AFE7225 in the L Band for Satellite Communications. Can somebody help?
Chandan Dutta,
A few things. The balun on the RX input path will not allow you to pass frequencies lower than 400kHz. The pass band is 400kHz to 800MHz.
Also, is your signal source coherent with with your clock source? Spectral skirting is likely…
Part Number: AFE7225EVM Hello,
I'm currently using the AFE7225 EVM with the evaluation GUI software (version 1.3) and I am noticing that on some of the RX Sync settings (under the Sync tab), the software seems to either be sending the data to the wrong…
Part Number: AFE7225 Other Parts Discussed in Thread: MSP430FR2433 , Hi,
In our design we are using AFE7225 for a custom SDR system. AFE 7225 is interfaced with MSP430FR2433 for programming registers set of AFE7225 at every boot. However, my changes from…
Hey Yusuf,
Thanks fo your interest. We are still waiting a response but we have also another issue. What is the input power dynamic range for ADC of AFE7225 and optimum input power, in dBm?
Regards,
Other Parts Discussed in Thread: AFE7225 looking for any layout recommendation for the AFE7225
The EVM files on the web only have the layers files without the DB file so I can`t check the constraint used and there is no layout section I can find on the…