Part Number: AFE7422EVM Other Parts Discussed in Thread: AFE7422 , LMK04828 Dear Vijay/Team,
We are trying to configure AFE7422 in Mode 7.
Our Required configuration parameters include,
LMFSHd - 24410 (Mode 7)
Interpolation - 36x
Decimation - 12x
Required…
Part Number: AFE7422EVM I use AFE7422EVM and TSW14J57
1 In Mode 3,capture wrong data
correct data
wrong data
2 In Mode 2,can not capture data
3 in Mode4,will never capture wrong data
Part Number: AFE7422EVM Other Parts Discussed in Thread: TSW14J57EVM I use the TSW14J57 rev E work with AFE7422EVM. I need to send a signal,and then capture another signal.
It should run continuously ,I use Matlab to control the process, refer to TSW14J57_PingPong_Example…
Part Number: AFE7422EVM Other Parts Discussed in Thread: AFE7422 I need an document or example or coding section of interfacing AFE7422 SPI with FT4232H in AFE7422EVM...Please provide a support
Part Number: AFE7422EVM Other Parts Discussed in Thread: AFE7422 Dear Vijay/Team,
Based on AFE7422 Schematic, the BALUN in Transmit and Receive path were listed below,
Component
Frequency Range Min (MHZ)
Frequency Range Max (MHZ)
Receive Path
TCM2…
Part Number: AFE7422EVM Other Parts Discussed in Thread: AFE7422 Hello TI Team,
We are trying to bring the AFE7422 using SPI. Please share the Register call back information of DAC and ADC reset buttons.
Thanks,
Preethika S
Part Number: AFE7422EVM Other Parts Discussed in Thread: AFE7422 Hello Team,
My Customer is looking to have a copy of the schematic of AFE7422EVM. Is this possible?
Thanks in advance.
Regards,
_Renan
Part Number: AFE7422EVM Other Parts Discussed in Thread: AFE7422 Hi team,
My customer is evaluating this part via the EVM and is confused by some differences in performances in the EVM and the part.
In the EVM (in contrast to the datasheet) it appears…
Part Number: AFE7422EVM Other Parts Discussed in Thread: TSW14J57EVM , AFE7422 Hello there,
We are evaluating AFE7422 with TSW14J57EVM. Configuring Mode 9 on both the boards, AFE7422 using GUI and TSW14J57EVM using HSDC Pro GUI.
Capturing in HSDC_Pro, the…