Part Number: AFE7769 Hi,
I'm working with the AFE7769.
I need to set the IF mixer NCO frequency for each TX/RX channel independently, but Macro 0x29 only exposes NCO control grouped by channel pairs / all channels:
Operand 1 (offset 0x00): NCO…
Part Number: AFE7769 We need to use the FB1 for DPD training with TX1 / TX2 / TX3 / TX4, and FB2 for sniffer function.
May I have the truth table for dual FB paths case of AFE7769 or AFE7769D, and the setting of TX QMC for different FB modes?
Part Number: AFE7769 Hi WI Team:
I want to configuration AFE7769 in Latte.
a). I haved executed setup.py.No error appears
b) I'm executing devInit.py. Error appears. Couldn't load iGUI.
c). I'm executiing basicBringup.py. Error appears. SPI…
Part Number: AFE7769D Other Parts Discussed in Thread: AFE7769 Setup
TXA and TXB share one analog LO (same PLL, one pair). I need them to transmit at two different RF frequencies, a small offset (a few MHz) apart, using the per-channel digital NCO/mixer…
Part Number: AFE7769 Hello,
We are working on our custom SDR
Our radio engineers have chosen a chip for our devices.
It will be AFE7769.
They ask if you can provide "S-parameters" files for AFE7769 RF in/out ports?
Could someone help me…
Part Number: AFE7769 Tool/software: When the TX_PLL of AFE7769 is set at 880MHz, a large power DC will be generated, and the QMC automatic calibration cannot go down, affecting the ACPR, this problem has a small probability, about 1/250, help to analyze…
Part Number: AFE7769-3P5EVM Other Parts Discussed in Thread: TSW14J58EVM , AFE7769DEVM , AFE7769D Tool/software: Can I get a user guide to interface AFE7769D-35EVM with TSW14J58EVM.
I searched over TI website, I could find the below document
1) Interfacing…
Part Number: AFE7769 Hi, We are using AFE7769 in our design as per out layout requirements we are Planning to place SSRF section in the following manner..
We are Planning to give isolation with shield on TOP and Bottom i.e (for TX & RX ) And ORX signal…
Part Number: AFE7769-3P5EVM Tool/software:
The errors I am getting are
1) AFE configuration in progress.
2) Could not detect FPGA Reset FTDI, Please reset FPGA manually.
Thanks and Regards,
Kalyan Giri