Part Number: AFE7906 AFE79xx_ConfigurationGuide_SBAA417_Jun2020.pdf The description of Parameter spiMode is 1.3-wire mode 1. 1-4 wire mode However, 0.3-wire mode Isn't it?
Part Number: AFE7906 Tool/software: Dear Texas,
Seems like every FSPI configurable pin is reserved in AFE7906 datasheet, is there another way we could use this functionality?
Thanks a lot,
Anna
Part Number: AFE7906 Other Parts Discussed in Thread: LMK04828 AFE7906 has 4 lanes per ADC as shown in the figure. Trying to connect.
sysParams.LMFSHdRx =["48410","48410","48410","48410"] sysParams.jesdTxLaneMux = [4,5,0,1,2,3,6,7]
If the above settings…
Part Number: AFE7906 Tool/software: Hi
I use AF7906 in my custom module
I tried to run the script AFE latte 2.6 version software where i will get 'Afe79xxPg1Format5.txt' .
But now i installed the latest version 2.8 here i am getting 'Afe79xxPg1Format5C…
Part Number: AFE7906
Tool/software:
Hi,
I went through the query in below link,
AFE7955: Maximum peak differential RF input power at device pins for DSA settings 0-3dB
based on the query, for AFE7906 at 2610MHz,
PFS_CW,min is -1.8dBm ~ 0.72Vpp…
Part Number: AFE7906 The configuration of the ADC used this time is Using 1 PLL and 2 ADCs Used as 4 lanes x 2 = 8 lanes.
The tolerance of REFCLK and SYSREF patterns of two ADCs is 0.1mm. I try to avoid errors as much as possible.
Adjust the sampling…
Part Number: AFE7906 Tool/software: I would like to know if the JESD204C IP by Texas Instruments is compatible with the Versal FPGA part number XCVP2802-VSVA5601. Additionally, are there any reference designs available for this combination?
Is the JESD204C…
Part Number: AFE7900EVM Tool/software: Hi
link : ://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1323838/afe7900evm-spi-interface
From the above trailing link, which we have already tested configuration using Stratix 10…
Part Number: AFE7906 Can u please provide upto what length it support for JESD204B lanes in board to board communication via FMC connectors ,and any timings constraints are there ???