Part Number: AFE7920EVM Hi Team,
We've been recently trying to connect the AFE7920EVM to a Kintex-7-like FPGA (XC7K410T) in a way indicated by the following schematic:
For the programming of the AFE EVM the attached script is being used (thanks to…
Part Number: AFE7920EVM Other Parts Discussed in Thread: AFE7950EVM Hi Team,
I was trying to use the AFE7920EVM and upon running the devInit.py script during the initialization stage I get the following errors:
cpldRegProg._pin0 : write failed
cpldRegProg…
Part Number: AFE7920EVM Hi Team,
I was wondering if there is a proper shutdown procedure or a Latte command to at least issue a reset of the AFE7920EVM?
I often see that even when I shut down Latte, the current drawn by the EVM is still around 5A, and…
Part Number: AFE7920EVM Hi Team,
I wanted to know if it is possible to disable GUI startup which is initiated from Latte when devInit.py script is run?
Currently we are not using the GUI, and we only use Latte for scripting the interaction with AFE evaluation…
Part Number: AFE7920EVM Hi Team,
This question is related to the one posted here: https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1189054/afe7920evm-afe7920evm-lmc-settings-issue
Currently, on a setup explained in the intro…
Part Number: AFE7920EVM Hi Team,
I've tried to modify the Repeater script (#5) which comes with Latte software for AFE7920EVM so its PLL works in distributed mode from an external clock source (@163.68 MHz).
The code (attached) manages to compile…
Part Number: AFE7920EVM Hi Team,
For a project I am working on, it is foreseen that 4 DACs of AFE7920EVM will output signals at 2245 MHz, 5020 MHz, 8212.5 MHz, and 6812.5 MHz, respectively, with the 32.5 MHz, 90 MHz, 375 MHz, and 375 MHz bandwidth, respectively…
Part Number: AFE7920EVM For a project I am currently involved with, we are using TI AFE7920EVM board, and I have some questions about the startup procedure of the said eval module.
Currently we do not have access to any pattern & capture hardware, such…
Part Number: AFE7920EVM Other Parts Discussed in Thread: AFE7920 , Hi,
I was wondering if it is possible to set up the AFE7920 eval board module in a repeater configuration, without FPGA board?
Kind regards,
Željko