Part Number: AFE7954 Tool/software: Dear TI,
Our engineer is using AFE7954 to design a high-speed acquisition card, could you provide one detailed DS to us.
Thank you.
Part Number: AFE7954 Hello,TI support Team
We are currently using the AFE7954.
We reviewed the datasheet section 7.3.11 (Temperature Sensor) and would like to use the on-chip temperature sensor. Our purpose is to monitor how much the die temperature…
Part Number: AFE7954 Tool/software: Dear TI Support Team,
Hello,
We are currently using the AFE7954 with the following configuration:
Fref = 491.52 MHz
Fdac = 11,796.48 MHz
DUC interpolation factor (ducFactorTx) = 48
Mode: Mixed Mode (2nd…
Part Number: AFE7954 sbaa729.pdf
Hello TI experts. On the Texas website, I found this document that discusses bringing up the afe79xx without using a microcontroller. Where can I find the HDL files for the module described in the document? I don't see…
Part Number: AFE7954 Hi Team,
We kindly request you to provide the .CSV file (Pin number, pin name, bank, and grouping) for the above mentioned part number.
Part Number: AFE7954 Other Parts Discussed in Thread: LMK04828 , AFE7950EVM Tool/software: Hi,
I use AFE7954 and LMK04828.
I made custom board.
I tried to connect between xilinx JESD IP and AFE, but it failed.
I used the following script and SPI…
Part Number: AFE7954 Tool/software: Hi
I use AF7954 and ZCU102.
I tried to program AFE but failed.
Below is the procedure I followed:
1. I run Latte( It seems to be called AFE79xx now )
2. Run setup.py (run->buffer)
3. Run devlnit.py (run…
Part Number: AFE7954 Other Parts Discussed in Thread: AFE7950EVM Tool/software: Hi, team
I use AFE7954
I want to enable SPIB
then, what values should I enter in SPIA?
can you let me know how to enable SPIB?
Regards,
Go Jeongju
Part Number: AFE7954 Tool/software: hi,
I use AFE7954 DAC
I can't use SPIA bacause I mapped it wrong.
so, Is it possible to control the DAC using only SPIB1?