Part Number: AFE8000 Tool/software: Please provide the data sheet for AFE8311C3RVBR. We are not considering this for a new design project. It is required for export procedures.
Part Number: AFE8000 Tool/software: Hello,
In case the device is planned to work on a harsh environment, what is the recommended termination for unused GPIO pins? (PU / PD / Float)
Best regards,
Avihay,
Hi Avihay,
For the RX model you will need to add a termination like in the image below as per the readme.
And make sure to add the S parameters for anything that your signal passes through, including the S4P provided with the model.
Best,
Camilo
Hi Haim,
Are you referring to configuring the AFE so that only 4 lanes are being used? If so then you can update the LMFS in the bringup script and then modify the lane mux parameter such that the top or bottom four SerDes lanes are used.
Regards,
…
Part Number: AFE8000 Tool/software: Hello,
The STX & SRX pins of P/N AFE8000 are routed to a connector, and will be used on a single board for two projects: In one project it will be connected to FPGA, and on the other one is will be floating. we…
Part Number: AFE8000 For simulation requirements needs we should have the internal RX and TX filters structure as detailed below:
The DUC interpolation filters coefficient for the two next scenarios:
375[MSPS] input signal that interpolating to 12…
Part Number: AFE8000 Tool/software: Hi,
I have several questions regarding the JTAG interface of the AFE8000 component:
1.) On the datasheet, TMS is mapped to G9 and TRST to R7:
On the EVB, TMS is connected to R7 and TRST to G9.
- Why there is a…
Part Number: AFE8000 Tool/software: Hi,
According to the AFE8000, unused SerDes_AMUX1 & 2 "can be left floating".
In case the component is planned to work in a harsh environment, do you recommend to keep these pins floating, or should I…
Part Number: AFE8000 Tool/software: Hi,
According to the AFE8000 datasheet, some of the Low Speed Digital I/Os are recommended for use only on certain balls:
Which GPIOs are recommended for use, In case I want to use 8x "NCO Select" (4x Rx, 4x Tx) &…