Hi Avihay,
As the power rails are tied to a common supply point we are not able to measure current separately. We recommend following the power supply groups given and using either the data provided in the datasheet or that measured on the EVM, using…
Hi Haim,
The software/design team commented that the hopping time for the AFE8000 should be in the same order as for the AFE79xx as presented in the app note.
Best,
Camilo
Part Number: AFE8000EVM Other Parts Discussed in Thread: AFE8000 Hi Guys,
We have VCK190 connected to EVM AFE8000 set up.
We are tring to activate JESD204C interface and we saw that sys_clk (375Mhz) is missing, it should come from the EVM AFE8000 via R317…
Hi Haim,
The AFE8000EVM GUI is not supported in the environment. What we suggest is to do instead is to use the AFE8000 GUI to produce a configuration file, which contains a list of SPI write/read checks/polls required to configure the part. In Linux…
Part Number: AFE8000 Hi,
Is there some additional info about the application of the AFE8000 for satellite communications? specifically from a radiation/enviromental tolerance point of view (LEO).
Thanks!
Part Number: AFE8000 Hi,
we are using AFE8000 devices.
I am a SW engineer, and I am looking for an information about:
1. Linux kernel version
2. Linux driver
3. Yocto recipe
Thanks
Part Number: AFE8000 For simulation requirements needs we should have the internal RX and TX filters structure as detailed below:
The DUC interpolation filters coefficient for the two next scenarios:
375[MSPS] input signal that interpolating to 12…
I used the following link to request the IP, it required filling in a spreadsheet with info on FPGA family and operating rates for the AFE8000. https://www.ti.com/tool/TI-JESD204-IP We have yet to receive the Vivado project, but it is reported as almost…
Hi Haim,
We have reached out through email in regards to creating the Versal + AFE8000 reference design. Once we have the response to our email we can share a completed reference design.
Regards,
David Chaparro