Part Number: AFE8000EVM Other Parts Discussed in Thread: TSW14J58EVM , AFE8000 , AFE7900EVM , AFE7900 Hi, I am asking a related question in regards to the HSDC Pro software.
My understanding is that the AFE8000EVM is not compatible with the HSDC Pro…
Part Number: AFE8000EVM Hello,
I am currently trying to change the NCO of AFE8000EVM dynamically. (I use zcu102 board and am bringing up the AFE using my firmware not your EVM software).
It doesn't need to change the frequency rapidly. So, I decided…
Part Number: AFE8000EVM Other Parts Discussed in Thread: AFE8000 , Hi,
I have two questions regarding the Tx chains of the AFE8000 EVM board:
(1) I've noticed that there are values differences of caps & inductors on the AFE8000EVM board matching…
Part Number: AFE8000EVM Hello,
We purchased the board of AFE8000EVM from Digikey. There are only four screws on the board, and two screws missing on the board, is it normal?
Pls help to suggest it.
Thanks,
Suri
Part Number: AFE8000EVM Other Parts Discussed in Thread: AFE8000 Hi,
I have the AFE8000EVM setup and configured correctly via the GUI and via scripts for our current needs.
What I want to do now is extract each of the internal register status and…
Part Number: AFE8000EVM Other Parts Discussed in Thread: AFE8000 Hi,
I've noticed that there are values differences of caps & inductors on the AFE8000EVM board matching network:
For example -
* (RXA_IN, J26) C410 equals 0.7pF, L76 equals 2.8nH,…
Part Number: AFE8000EVM Other Parts Discussed in Thread: LMK04828 , AFE8000 I'm bring up the AFE8000EVM board, matched with the VPK120 board from Xilinx.
Synthesis of the FPGA using the reference design you provided seems to work.
However when I download…
Part Number: AFE8000EVM Other Parts Discussed in Thread: AFE7900EVM , AFE8000 , AFE7900 Hi,
I'm trying to bring up the AFE8000EVM platform, connected to a Xilinx VPK120 board, with a reference image supplied by TI.
I have few questions regarding…
Part Number: AFE8000EVM Other Parts Discussed in Thread: TSW14J58EVM , AFE8000
Hi TI,
I am currently running though the bring up process as provided with the AFE8000 connected to the TSW14J58EVM.
The Input ref signal to the LMK on the AFE8000…