Other Parts Discussed in Thread: OMAP-L137 , AM1705 Hello,
I'm using the sfh_OMAP-L137.exe to flash images to external SPI flash for my custom AM1705 board.
When using the application as shown below:
C:\flasher>sfh_OMAP-L137.exe -flash <UBL binary…
Hello guys,
I'm in the process of building U-boot nad linux for my custom board. I would like to know if Sourcery Codebench can be used instead of codesourcery g++ lite because the latter is not available.
Best regards,
Patricio
Other Parts Discussed in Thread: AM1705 Hi there,
I'm having issues powering up the EMIFA peripheral through the GEL Script for an AM1705. I've attached my current GEL Script with the PSC0_lPSC_enable(0,3) uncommented out. When it is run like this I get…
Other Parts Discussed in Thread: AM1705 , TLV320AIC3106 , TPS65023 , OMAP-L137 , OMAPL138 , OMAP-L138 Hello guys,
First of all, my board has the following hardware:
CPU: AM1705 SPI Flash : K0XMFI011 (Spansion) - 4MBytes - Connected to SPI0 Nand Flash: S34ML01G200TFI000…
One more thing, DA830(OMAPL137) /AM1705/AM1707 boards doesn't have much documentation but OMAPL138.
You can refer to OMAPL138 documentation & wiki pages but you should change the file name like da850evm.h to da830evm.h
also, board-da850-evm.c…
Other Parts Discussed in Thread: OMAP-L137 , AM1705 , OMAP-L138 Hello,
I have several doubts regarding the Serial Flash and Boot utils. My questions are the following:
I'm using the OMAP-L137_FlashAndBootUtils_2_40 version.
1) How do I know if I need…
Other Parts Discussed in Thread: AM1705 Hello,
I'm using the IBIS file sprm491a.zip available in the AM1705 page.
When using it with Hyperlynx, you can notice that the pin numbering is for a BGA package, however this MPU comes in a QFP package.
Also…
Other Parts Discussed in Thread: AM1705 , AM1707 Hello,
I'm working on a design with the AM1705. I'm looking right now for a PHY chip that is compatible with this processor. I have seen discussions where some people say that the AM1705 is incompatible with…
Other Parts Discussed in Thread: AM1705 Hello Titus and all,
I'm using DaVinci-PSP-SDK-03.22.00.04.
I haven't been able to make U-boot to detect the LAN8720A PHY IC . I'm using an external 50MHz clock gen connected to both the LAN8720A and the AM1705…
Other Parts Discussed in Thread: AM1705 Hello,
I'm right know designing the SDRAM section for the AM1705. I'm trying to use the IBIS file available on the AM1705 product page with Hyperlynx for studying signal integrity between the MPU and SDRAM…