Other Parts Discussed in Thread: AM1802 , TPS650061 , AM1808 , OMAP-L138 , OMAPL138 I've got a new board built for the first time and am trying to debug why it isn't showing any real signs of life.
I've confirmed the power rails are correct and come…
Other Parts Discussed in Thread: AM1808 , OMAP-L138 , AM1802 , OMAPL138 Hello:
I've successfully booted our new board using AISgen to modify a stock u-boot-bin as well as boot a kernel and filesystem. I've followed many Wikis to get to this point and my Host…
Other Parts Discussed in Thread: AM1808 , OMAP-L138 , SYSBIOS , MATHLIB , OMAPL138 , AM1802 We are about to bring up a new board and just realized that booting from a SD Card isn't quite as straight forward as we thought. We didn't design in SPI Flash but have…
Other Parts Discussed in Thread: AM1802 Hi,
I have a AM1802 target board using SPI1 FLASH boot. I have set the boot mode pins as SPI1 FLASH mode, and the board was used to be booted successfully. Then I measured the SPI pins, OSCIN, OSCOUT, and boot mode…
Other Parts Discussed in Thread: AM1802 , AM1808 , AM1806 I believe it can but I wanted to confirm that the AM1802 can have a I2S port (to connect to an external DAC) as well as a DIT (to connect to an external S/PDIF transmitter) and both can be active…
Other Parts Discussed in Thread: AM1802 , AM1808 , OMAPL138 Hello,
I have a XDS220 card which has an AM1802 chip on it. I want to try how the EMAC works. I connected to AM1802 via an emulator and I don't have a GEL file to initialize the DDR. Can anybody…
Other Parts Discussed in Thread: AM1802 Hi, I plan to use Boundary scan for production testing of the DDR interface with AM1802 processor. Please let me know
1. How Can I implement this?
2. What are the limitations of using Boundary scan for DDR with…
Other Parts Discussed in Thread: AM1802 When we debug the AM1802,the power sequence is 1.2V->1.8v->3.3V.When the 1.2V power up,we can test a 1.3V on 3.3V power pin. We disconnect the 3.3V power,the 1.3V still
exist.Remove all the outside devices…
Other Parts Discussed in Thread: AM1808 , AM1802 I posted this question at the bottom of a related thread but got no response. I'm really stuck on this one so I'm giving it its own thread:
I have CCS5 for Linux installed on Ubuntu 10.10.
In general…
Other Parts Discussed in Thread: AM1802 I'm looking at the Am1802 SDRAM interface on EMIFA and not clear on a couple items. We are currently working with an Atmel AT91SAM9260 which has a 32bit SDRAM data bus which we use to connect (2) 256MBit x 16…