Part Number: AM2632 Hi,
I am using AM2632 MCSPI in FIFO mode to communicate with a ADC. The ADC requires 420 ns delays between SPI words. How can I configure the MCSPI in FIFO mode to insert a delay of 420 ns between de-assertion of chip select line and…
Part Number: AM2632 Hello,
we are using AM2632 and I have a question about the possiblities of bootflow. We use the AM2632 in lockstep mode, so we have two available cores (R5SS0 and R5SS1) Is it possible to load firmware to R5SS1 from SBL and then start…
D Bennett said: I am selecting a processor for an embedded engine controller that will require PRP ethernet communications. Two physical ethernet connections with the same IP and MAC address (per PRP requirements). Speed is 10/100 (Gbit not required). Data…
Part Number: AM2632 Hi Team,
When using a GPIO Interrupt triggering on Rising and Falling edge, when you get an interrupt is there a good way to differentiate a rising edge or a falling edge other than polling the GPIO pin itself?
Thanks!
-Jack
Part Number: AM2632 I can understand the point that it is not possible nor wanted that someone is running the AES decryption in Flash. I was under the impression that the image will be loaded to RAM and the encryption and the certificate check will be…
Part Number: AM2632 Hi,
I have a question about OE_Override and IE_Override settings in MSS_IOMUX Registers. I have configured a pin as GPIO output and toggles the output every 500 ns. I have noticed that when the OE_OVERRIDE and OE_OVERRIDE_CTRL are …
Part Number: AM2632-Q1
Hi team,
Is it possible to connect the external SRAM memory to AM2632-Q1? My customer would like to enhance the memory capacity.
If it is possible, how much the customer can add SRAM memory?
Best regards,
Shunsuke Yamamoto
Part Number: AM2632-Q1 Hello,Expert.
We are currently developing an ECU prototype. I would like to start evaluating Sitara's power supply circuit and heat dissipation structure immediately, but I do not yet have product-level test software.
For example…
Michael Shklyarman said: Or they need to add EXTPHY following instructions from Adding Support for Custom PHY in the User Guide.
They will need to follow the steps mentioned in the guide:
AM263x MCU+ SDK: Enet Migration Guide
Since the driver for the dp83867…