Part Number: AM26LV31E-EP Hello.
In the datasheet of AM26LV31E-EP the max input current is 10[uA].
1.does this means that if i want to use pull up resistor the maximum current through each pin is 10[uA]?
Another Q:
2.the parameters IOH,IOL - does this…
Part Number: AM26LV31E-EP Other Parts Discussed in Thread: AM26LV31E I am designing Hardware using AM26LV31E-EP. I need reference schematic or application note for the same. Kindly help me out.
Part Number: AM26LV31E-EP Other Parts Discussed in Thread: AM26LV31E , AM26LV31 Hi,
we are having two modules each module is having am26lv31e driver which drives rs485 signals. at the destination there is single receiver. our application is such that one…
Part Number: AM26LV31E-EP Other Parts Discussed in Thread: AM26C31-EP Hi,
I need a similar compatible part that is 5V operation.
What do you recommend?
Thanks,
HSG
Part Number: AM26LV31E-EP Hi Team, we would like to clarify the operating free-air temperature range on the datasheet. The values on the absolute maximum rating and the recommended operating condition are the same. Does this mean the if the device operates…
Part Number: AM26LV31E-EP Other Parts Discussed in Thread: AM26C31 , AM26C31M Hi there,
I want to know about the maximum differential input voltage of AM26LV31E-EP, but information about the maximum differential input voltage is not shown on the AM26LV31E…
Part Number: AM26LV31E-EP Other Parts Discussed in Thread: AM26LV31E , SN65LBC174A-EP , SN65HVD30-EP , SN65HVD10-EP , SN65HVD12-EP , SN55HVD75-EP , AM26LV31 Hi,
I implement RS-422 interface using AM26LV31E-EP, and I am worried about the lightning protection…
Part Number: AM26LV31E-EP In an electronic board we are using the AM26LV31E-EP differential line driver.
For the LIGHTNING qualification test, we need to inject a burst of voltage pulses (in both polarities) into the individual outputs of the AM26LV31E…